<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックMemory error injection Test in eTPU</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Memory-error-injection-Test-in-eTPU/m-p/658846#M7162</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;I am working on SDM and SCM&amp;nbsp;memory error injection and correction test for&amp;nbsp;eTPU . This is for MPC5676RRM . I am trying to understand the usage of "eTPU Data Error Injection Address Register&amp;nbsp;" . This register descriptions says to use a 12 bit address but the memory map for SDM shows as 0x8000-0xBFFF which&amp;nbsp;are 16 bit addresses . So not sure how to configure this register to inject fault in SDM .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also which register I should use for doing a memory pattern test for eTPU ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a sample code I can refer to for the two above ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Arjun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 May 2017 14:16:33 GMT</pubDate>
    <dc:creator>arjunrath</dc:creator>
    <dc:date>2017-05-02T14:16:33Z</dc:date>
    <item>
      <title>Memory error injection Test in eTPU</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Memory-error-injection-Test-in-eTPU/m-p/658846#M7162</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;I am working on SDM and SCM&amp;nbsp;memory error injection and correction test for&amp;nbsp;eTPU . This is for MPC5676RRM . I am trying to understand the usage of "eTPU Data Error Injection Address Register&amp;nbsp;" . This register descriptions says to use a 12 bit address but the memory map for SDM shows as 0x8000-0xBFFF which&amp;nbsp;are 16 bit addresses . So not sure how to configure this register to inject fault in SDM .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also which register I should use for doing a memory pattern test for eTPU ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a sample code I can refer to for the two above ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Arjun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 May 2017 14:16:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Memory-error-injection-Test-in-eTPU/m-p/658846#M7162</guid>
      <dc:creator>arjunrath</dc:creator>
      <dc:date>2017-05-02T14:16:33Z</dc:date>
    </item>
    <item>
      <title>Re: Memory error injection Test in eTPU</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Memory-error-injection-Test-in-eTPU/m-p/658847#M7163</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;0x8000-0xBFFF is address offset only.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Address ranges from CPU side are&lt;/P&gt;&lt;P&gt;eTPU_AB 0xC3FC8000 - 0xC3FC97FF&lt;/P&gt;&lt;P&gt;eTPU_C 0xC3E28000 - 0xC3E28BFF&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The two least significant bits are 0 (read-only), so that the address is always 32-bit aligned.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Currently I don’t have example code for this. However, it seems quite straightforward, similar way as common ECC RAM by ECSM module as described in AN5200, section 6.1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See RM screenshot below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19418i57DB144E597DAEC1/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2017 12:35:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Memory-error-injection-Test-in-eTPU/m-p/658847#M7163</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2017-05-04T12:35:40Z</dc:date>
    </item>
  </channel>
</rss>