<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5746R SPI Problem in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5746R-SPI-Problem/m-p/658718#M7161</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Qiao,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the MPC5746R’s DSPI0 is a Master and communicates with two peripherals/Slaves.&lt;/P&gt;&lt;P&gt;What is the connection? Can you share schematic? What is your DSPI initialization and TX/RX code?&lt;/P&gt;&lt;P&gt;Could you also post what is really seen on SPI lines for a mentioned frames?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Feb 2017 13:15:39 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2017-02-22T13:15:39Z</dc:date>
    <item>
      <title>MPC5746R SPI Problem</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5746R-SPI-Problem/m-p/658717#M7160</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I have two peripherals both of which are slave of DSPI_0. When only one of them works， I can read the right data from the SPI. But if I&amp;nbsp;transfer data to peripheral B through SPI after peripheral A have just finished its job , &amp;nbsp;I can not read the right data from the SPI. &amp;nbsp;Where can the problem come from ?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Qiao&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 02:33:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5746R-SPI-Problem/m-p/658717#M7160</guid>
      <dc:creator>qiaodeng</dc:creator>
      <dc:date>2017-02-22T02:33:59Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5746R SPI Problem</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5746R-SPI-Problem/m-p/658718#M7161</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Qiao,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the MPC5746R’s DSPI0 is a Master and communicates with two peripherals/Slaves.&lt;/P&gt;&lt;P&gt;What is the connection? Can you share schematic? What is your DSPI initialization and TX/RX code?&lt;/P&gt;&lt;P&gt;Could you also post what is really seen on SPI lines for a mentioned frames?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 13:15:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5746R-SPI-Problem/m-p/658718#M7161</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-02-22T13:15:39Z</dc:date>
    </item>
  </channel>
</rss>