<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: ULPI to HSIC Bridge</title>
    <link>https://community.nxp.com/t5/MPC5xxx/ULPI-to-HSIC-Bridge/m-p/655555#M7049</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I did check with Microchip and they don't have a part like that either. So it must only exist as an IP block for now.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Steve&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Feb 2017 14:38:46 GMT</pubDate>
    <dc:creator>nextsteve</dc:creator>
    <dc:date>2017-02-22T14:38:46Z</dc:date>
    <item>
      <title>ULPI to HSIC Bridge</title>
      <link>https://community.nxp.com/t5/MPC5xxx/ULPI-to-HSIC-Bridge/m-p/655551#M7045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I found this app note relating to trends in USB in automotive:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2Ftraining%2Fdoc%2Fftf%2F2014%2FFTF-AUT-F0335.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/training/doc/ftf/2014/FTF-AUT-F0335.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In particular, I found this quote:&lt;/P&gt;&lt;P&gt;There are HSIC-to-ULPI transceivers that provide HSIC functionality to standard USB 2.0 devices.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is the HSIC to ULPI transceiver a real component? If so could someone give me a part number?&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Steve&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Feb 2017 06:08:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/ULPI-to-HSIC-Bridge/m-p/655551#M7045</guid>
      <dc:creator>nextsteve</dc:creator>
      <dc:date>2017-02-21T06:08:55Z</dc:date>
    </item>
    <item>
      <title>Re: ULPI to HSIC Bridge</title>
      <link>https://community.nxp.com/t5/MPC5xxx/ULPI-to-HSIC-Bridge/m-p/655552#M7046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steve, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HSIC does not act like a ‘normal’ USB chip, it is High Speed only.&amp;nbsp; So, it probably does not make sense to convert from HSIC to ULPI.&amp;nbsp; If you want to add more HSIC connections, an HSIC hub would probably be better because the hub adds flow/speed control downstream. Note that HSIC is really only meant to be a high speed connection between devices on the same PCB so be sure to keep the traces short to avoid noise issues.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I suspect that the actual desire is to add additional USB ports to the design.&amp;nbsp; If that is the case, why not look at a USB hub to add the extra ports?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If there is a concern with regards to bandwidth, I would recommend using the i.MX6D/Q Plus.&amp;nbsp; The i.MX6Dual/Quad Plus has a bit more streamlined internal routing of the DDR which will aid in overall throughput.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Lydia&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Feb 2017 20:43:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/ULPI-to-HSIC-Bridge/m-p/655552#M7046</guid>
      <dc:creator>lydia_ziegler</dc:creator>
      <dc:date>2017-02-21T20:43:13Z</dc:date>
    </item>
    <item>
      <title>Re: ULPI to HSIC Bridge</title>
      <link>https://community.nxp.com/t5/MPC5xxx/ULPI-to-HSIC-Bridge/m-p/655553#M7047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lydia thanks for responding. You are definitely the most helpful IMX6 support person I've encountered so I'm glad you're online.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The actual desire is to convert the USB ULPI interface on my MPC5xxx to HSIC so I can directly interface it to one of the HSIC USB Hosts on my IMX6 instead of using a ULPI USB transceiver IC to the IMX6 OTG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The bullet point I found on that automotive USB presentation sounded exactly like what I needed so I was wondering if that was an actual component I could buy and use or if it is a theoretical thing that is possible. I see a different company sells ULPI-HSIC as an HDL IP block but I want an actual component.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Steve&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Feb 2017 21:10:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/ULPI-to-HSIC-Bridge/m-p/655553#M7047</guid>
      <dc:creator>nextsteve</dc:creator>
      <dc:date>2017-02-21T21:10:06Z</dc:date>
    </item>
    <item>
      <title>Re: ULPI to HSIC Bridge</title>
      <link>https://community.nxp.com/t5/MPC5xxx/ULPI-to-HSIC-Bridge/m-p/655554#M7048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the extra info, that makes sense.&amp;nbsp; Have you checked with Microchip?&amp;nbsp; They would probably be your best bet for an HSIC -&amp;gt; ULPI converter chip since they have acquired SMSC.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 14:12:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/ULPI-to-HSIC-Bridge/m-p/655554#M7048</guid>
      <dc:creator>lydia_ziegler</dc:creator>
      <dc:date>2017-02-22T14:12:55Z</dc:date>
    </item>
    <item>
      <title>Re: ULPI to HSIC Bridge</title>
      <link>https://community.nxp.com/t5/MPC5xxx/ULPI-to-HSIC-Bridge/m-p/655555#M7049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I did check with Microchip and they don't have a part like that either. So it must only exist as an IP block for now.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Steve&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 14:38:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/ULPI-to-HSIC-Bridge/m-p/655555#M7049</guid>
      <dc:creator>nextsteve</dc:creator>
      <dc:date>2017-02-22T14:38:46Z</dc:date>
    </item>
    <item>
      <title>Re: ULPI to HSIC Bridge</title>
      <link>https://community.nxp.com/t5/MPC5xxx/ULPI-to-HSIC-Bridge/m-p/655556#M7050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you have a SPI port available?&amp;nbsp; You can get fairly high speeds to do inter processor communication.&amp;nbsp; Maybe that would be an option to consider.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Lydia&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 15:50:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/ULPI-to-HSIC-Bridge/m-p/655556#M7050</guid>
      <dc:creator>lydia_ziegler</dc:creator>
      <dc:date>2017-02-22T15:50:06Z</dc:date>
    </item>
    <item>
      <title>Re: ULPI to HSIC Bridge</title>
      <link>https://community.nxp.com/t5/MPC5xxx/ULPI-to-HSIC-Bridge/m-p/655557#M7051</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Preference of my software programmers to use USB over SPI due to Linux driver support.&lt;/P&gt;&lt;P&gt;USB is a bad interchip embedded interface so that's why I'm exploring HSIC.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Steve&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 16:24:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/ULPI-to-HSIC-Bridge/m-p/655557#M7051</guid>
      <dc:creator>nextsteve</dc:creator>
      <dc:date>2017-02-22T16:24:28Z</dc:date>
    </item>
  </channel>
</rss>