<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPC5746R Flash Problem in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5746R-Flash-Problem/m-p/652796#M6895</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I am debugging MPC5746R with S32 Studio. I can only debug z4_1 successfully. If I flash z4_0, it will show the error:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Error in ONCE status register during instruction execution.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Also I am confused about the project name when I create a new project:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="170973_170973.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/122605iFDADFDBF48649FFD/image-size/large?v=v2&amp;amp;px=999" role="button" title="170973_170973.png" alt="170973_170973.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10952iAFD3CC886F04425E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;According to the start address, it seems that the project Test_Z4_1 corresponds to the core Z4_0, and the name can't be changed. Could somebody explain this ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Qiao&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Dec 2016 07:37:34 GMT</pubDate>
    <dc:creator>qiaodeng</dc:creator>
    <dc:date>2016-12-06T07:37:34Z</dc:date>
    <item>
      <title>MPC5746R Flash Problem</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5746R-Flash-Problem/m-p/652796#M6895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I am debugging MPC5746R with S32 Studio. I can only debug z4_1 successfully. If I flash z4_0, it will show the error:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Error in ONCE status register during instruction execution.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Also I am confused about the project name when I create a new project:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="170973_170973.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/122605iFDADFDBF48649FFD/image-size/large?v=v2&amp;amp;px=999" role="button" title="170973_170973.png" alt="170973_170973.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10952iAFD3CC886F04425E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;According to the start address, it seems that the project Test_Z4_1 corresponds to the core Z4_0, and the name can't be changed. Could somebody explain this ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Qiao&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Dec 2016 07:37:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5746R-Flash-Problem/m-p/652796#M6895</guid>
      <dc:creator>qiaodeng</dc:creator>
      <dc:date>2016-12-06T07:37:34Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5746R Flash Problem</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5746R-Flash-Problem/m-p/652797#M6896</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Qiao,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Z4_0 is the core, which MPC5746R boot from. It does not matter which address you use for Z4_0 and Z4_1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to load core for both cores via LaunchGroup and it works correct. I also tried to load code for Z4_0 and it works correct,&lt;/P&gt;&lt;P&gt;It not possible to debug Z4_1 without Z4_0. Z4_0 project loads code for both cores and Z4_1 only attach itself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Dec 2016 10:00:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5746R-Flash-Problem/m-p/652797#M6896</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2016-12-06T10:00:00Z</dc:date>
    </item>
  </channel>
</rss>