<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC 5604C EE Driver in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC-5604C-EE-Driver/m-p/399835#M662</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ECC protection cannot be disabled. Core reading or executing of data affected by multibit ECC error always lead in IVOR1/2/3 or checkstop state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See following document, chapter 3.1:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-103300"&gt;https://community.freescale.com/docs/DOC-103300&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ECC error just may happen and must be handled. Let me name some possible reasons of FLASH non-correctable ECC error reason (not necessarily related to EE handler):&lt;/P&gt;&lt;P&gt;- Unexpected reset during flash erase or flash program operation&lt;/P&gt;&lt;P&gt;- Wear out of particular flash sector = number of program/erase cycles that device’s flash is capable to withstand is exceded (in practice, real endurance is greater than specified minimum).&lt;/P&gt;&lt;P&gt;- Over-programming of particular flash area that is programming without erasing. It is basically software fault.&lt;/P&gt;&lt;P&gt;- Soft error (radiation, electro-magnetic interference, or electrical noise) during reading or executing from flash memory&lt;/P&gt;&lt;P&gt;- In general fault due to damage caused by running the device out of spec whatever way.&lt;/P&gt;&lt;P&gt;- and finally FLASH ECC error may be intentionally generated by ECC error injection.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Sep 2015 06:55:19 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2015-09-23T06:55:19Z</dc:date>
    <item>
      <title>MPC 5604C EE Driver</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC-5604C-EE-Driver/m-p/399834#M661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using freescale ee driver for mpc 5604C in my app which uses IVOR 2 exception handler to recover ECC error in Flash. I don't want any exception handlers triggering interrupts in bootloader. Can anyone please, suggest a possible way to use the EE driver or alternative to cope without exception handlers?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Sep 2015 10:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC-5604C-EE-Driver/m-p/399834#M661</guid>
      <dc:creator>gsb_selvam</dc:creator>
      <dc:date>2015-09-22T10:04:50Z</dc:date>
    </item>
    <item>
      <title>Re: MPC 5604C EE Driver</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC-5604C-EE-Driver/m-p/399835#M662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ECC protection cannot be disabled. Core reading or executing of data affected by multibit ECC error always lead in IVOR1/2/3 or checkstop state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See following document, chapter 3.1:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-103300"&gt;https://community.freescale.com/docs/DOC-103300&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ECC error just may happen and must be handled. Let me name some possible reasons of FLASH non-correctable ECC error reason (not necessarily related to EE handler):&lt;/P&gt;&lt;P&gt;- Unexpected reset during flash erase or flash program operation&lt;/P&gt;&lt;P&gt;- Wear out of particular flash sector = number of program/erase cycles that device’s flash is capable to withstand is exceded (in practice, real endurance is greater than specified minimum).&lt;/P&gt;&lt;P&gt;- Over-programming of particular flash area that is programming without erasing. It is basically software fault.&lt;/P&gt;&lt;P&gt;- Soft error (radiation, electro-magnetic interference, or electrical noise) during reading or executing from flash memory&lt;/P&gt;&lt;P&gt;- In general fault due to damage caused by running the device out of spec whatever way.&lt;/P&gt;&lt;P&gt;- and finally FLASH ECC error may be intentionally generated by ECC error injection.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Sep 2015 06:55:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC-5604C-EE-Driver/m-p/399835#M662</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2015-09-23T06:55:19Z</dc:date>
    </item>
  </channel>
</rss>