<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic AN4224 Trace support on MPC5744P for code coverage analysis in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/AN4224-Trace-support-on-MPC5744P-for-code-coverage-analysis/m-p/398194#M642</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are no Aurora pins available on the 144 pin package of MPC5744P.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="48574_48574.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120465i1976E0E757A2F738/image-size/large?v=v2&amp;amp;px=999" role="button" title="48574_48574.jpg" alt="48574_48574.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pic1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55182i842C00D124524FB2/image-size/large?v=v2&amp;amp;px=999" role="button" title="pic1.jpg" alt="pic1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When looking at Table-1 and Figure-1 in AN4224 does that mean that tracing through JTAG TAP (without using MDO pins) is not possible with MPC5744P in LQFP144?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="48578_48578.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120466i59918C1F65C16652/image-size/large?v=v2&amp;amp;px=999" role="button" title="48578_48578.PNG" alt="48578_48578.PNG" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pic2.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55220iD1BA79C0D603AE61/image-size/large?v=v2&amp;amp;px=999" role="button" title="pic2.PNG" alt="pic2.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For instance when someone wants to do code coverage analysis then the NPC Auxiliary Port has to be used on LQFP144 - which will be slower than Aurora or move to BGA257 where the high speed trace capabilities through Aurora is available. Is my assumption right?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;br&lt;/P&gt;&lt;P&gt;Guenter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Jul 2015 16:01:26 GMT</pubDate>
    <dc:creator>guenter_loettrich</dc:creator>
    <dc:date>2015-07-09T16:01:26Z</dc:date>
    <item>
      <title>AN4224 Trace support on MPC5744P for code coverage analysis</title>
      <link>https://community.nxp.com/t5/MPC5xxx/AN4224-Trace-support-on-MPC5744P-for-code-coverage-analysis/m-p/398194#M642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are no Aurora pins available on the 144 pin package of MPC5744P.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="48574_48574.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120465i1976E0E757A2F738/image-size/large?v=v2&amp;amp;px=999" role="button" title="48574_48574.jpg" alt="48574_48574.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pic1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55182i842C00D124524FB2/image-size/large?v=v2&amp;amp;px=999" role="button" title="pic1.jpg" alt="pic1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When looking at Table-1 and Figure-1 in AN4224 does that mean that tracing through JTAG TAP (without using MDO pins) is not possible with MPC5744P in LQFP144?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="48578_48578.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120466i59918C1F65C16652/image-size/large?v=v2&amp;amp;px=999" role="button" title="48578_48578.PNG" alt="48578_48578.PNG" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pic2.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55220iD1BA79C0D603AE61/image-size/large?v=v2&amp;amp;px=999" role="button" title="pic2.PNG" alt="pic2.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For instance when someone wants to do code coverage analysis then the NPC Auxiliary Port has to be used on LQFP144 - which will be slower than Aurora or move to BGA257 where the high speed trace capabilities through Aurora is available. Is my assumption right?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;br&lt;/P&gt;&lt;P&gt;Guenter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jul 2015 16:01:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/AN4224-Trace-support-on-MPC5744P-for-code-coverage-analysis/m-p/398194#M642</guid>
      <dc:creator>guenter_loettrich</dc:creator>
      <dc:date>2015-07-09T16:01:26Z</dc:date>
    </item>
    <item>
      <title>Re: AN4224 Trace support on MPC5744P for code coverage analysis</title>
      <link>https://community.nxp.com/t5/MPC5xxx/AN4224-Trace-support-on-MPC5744P-for-code-coverage-analysis/m-p/398195#M643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the meantime I've got feedback from the automotive apps team, thanks to Randy Dees:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"The Nexus standard allows for multiple types of external&lt;BR /&gt;trace interfaces. Specifically, it allows for a parallel trace interface&lt;BR /&gt;(defined in all revisions of the IEEE-ISTO 5001 standard) and the high-speed&lt;BR /&gt;serial trace interface, that utilizes the Aurora transport mechanism (added in&lt;BR /&gt;the IEEE-ISTO 5001-2012 version of the standard).&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The 144 pin package does have access to a 4-bit parallel&lt;BR /&gt;Nexus trace interface (MDO). This does allow limited trace bandwidth for code&lt;BR /&gt;coverage analysis. Branch history mode may need to be selected in the tool due&lt;BR /&gt;to the limited bandwidth available with the 4-bit MDO parallel Nexus interface.&lt;BR /&gt;Branch History mode does allow the tool to determine if all branches had been&lt;BR /&gt;executed (taken/not taken) for code coverage. If more detailed trace&lt;BR /&gt;information is required, then the larger package would have to be used. For&lt;BR /&gt;some products, Freescale does have adapters available that allows access to the&lt;BR /&gt;high-speed Aurora Nexus interface by using the larger package and fitting into&lt;BR /&gt;the smaller package footprint. Unfortunately, this type of adapter is not&lt;BR /&gt;currently available for the MPC5744P.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The trace data is never accessible via JTAG port of the&lt;BR /&gt;MPC5744P. That would require the trace to memory option, which is not&lt;BR /&gt;implemented on the MPC5744P (as shown in Table 1 of the application note). This&lt;BR /&gt;is also shown in Figure 1 of the application note, although this may not be&lt;BR /&gt;clear. In figure 1 it does not define the difference between the heavy&lt;BR /&gt;dark/black "bus" (JTAG control) and the heavy grey "bus' that is&lt;BR /&gt;the Nexus trace data. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The customer should refer to AN2614 "MPC553x,&lt;BR /&gt;MPC555x, and MPC556x Family Nexus Interface Connector" or AN3968&lt;BR /&gt;"Nexus Interface Connector for the MPC567xF and MPC5676R Families"&lt;BR /&gt;for recommended pin-outs of the parallel Nexus interface. For the 4-bit&lt;BR /&gt;parallel Nexus interface, usually, the 32-pin MICTOR connector is used,&lt;BR /&gt;however, the 50-pin SAMTEC may also be used if the customer uses the same tools&lt;BR /&gt;for devices that support the 16-bit parallel Nexus interface. (Normally, the&lt;BR /&gt;MICTOR is recommended for 4 to 12-bit MDO pins [AN2614 and AN3968] and the&lt;BR /&gt;SAMTEC 50-pin for 12 to 16-bit MDO devices [AN3968]). "&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jul 2015 08:32:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/AN4224-Trace-support-on-MPC5744P-for-code-coverage-analysis/m-p/398195#M643</guid>
      <dc:creator>guenter_loettrich</dc:creator>
      <dc:date>2015-07-17T08:32:53Z</dc:date>
    </item>
  </channel>
</rss>