<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 MPC5775K Library usage in S32DS</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-Library-usage-in-S32DS/m-p/641651#M6378</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Customer want to use SPE2 intrinsic functions for MPC5775K in S32DS.&lt;/P&gt;&lt;P&gt;Thus customer choose "newlib" in "Target Processor =&amp;gt; Libraries Support". The SPE intrinsic functions can be used now.&lt;/P&gt;&lt;P&gt;But the "newlib" doesn't include some math functions like asin/acos in ewl library.&lt;/P&gt;&lt;P&gt;What's the recommended method to add the ewl library into the S32DS project besides "newlib"?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jason Yang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Apr 2017 14:16:03 GMT</pubDate>
    <dc:creator>jinjingyang</dc:creator>
    <dc:date>2017-04-25T14:16:03Z</dc:date>
    <item>
      <title>MPC5775K Library usage in S32DS</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-Library-usage-in-S32DS/m-p/641651#M6378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Customer want to use SPE2 intrinsic functions for MPC5775K in S32DS.&lt;/P&gt;&lt;P&gt;Thus customer choose "newlib" in "Target Processor =&amp;gt; Libraries Support". The SPE intrinsic functions can be used now.&lt;/P&gt;&lt;P&gt;But the "newlib" doesn't include some math functions like asin/acos in ewl library.&lt;/P&gt;&lt;P&gt;What's the recommended method to add the ewl library into the S32DS project besides "newlib"?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jason Yang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Apr 2017 14:16:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-Library-usage-in-S32DS/m-p/641651#M6378</guid>
      <dc:creator>jinjingyang</dc:creator>
      <dc:date>2017-04-25T14:16:03Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775K Library usage in S32DS</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-Library-usage-in-S32DS/m-p/641652#M6379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jason,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is not possible to use both libraries newlib and EWL in one project. But there is a solution in form of ammclib. It contains optimized trigonometric functions and it is easy to include this library to project in S32DS. In installation folder in section doc, there is a document which describes, how to integrate this library to the project. Please look and let me know if it is suitable for your customer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can download the ammclib at the following URL:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cache.nxp.com/assets/downloads/data/en/libraries/MPC577xK_AMMCLIB_v1.1.7_LIB.exe?fsrch=1&amp;amp;sr=9&amp;amp;pageNum=2" title="http://cache.nxp.com/assets/downloads/data/en/libraries/MPC577xK_AMMCLIB_v1.1.7_LIB.exe?fsrch=1&amp;amp;sr=9&amp;amp;pageNum=2"&gt;http://cache.nxp.com/assets/downloads/data/en/libraries/MPC577xK_AMMCLIB_v1.1.7_LIB.exe?fsrch=1&amp;amp;sr=9&amp;amp;pageNum=2&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Apr 2017 09:02:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-Library-usage-in-S32DS/m-p/641652#M6379</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2017-04-26T09:02:00Z</dc:date>
    </item>
  </channel>
</rss>