<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: Using Ethernet port for alternate functionality</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Using-Ethernet-port-for-alternate-functionality/m-p/640502#M6293</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;If the MPC5200B Ethernet is configured using the &lt;SPAN style="color: black;"&gt;GPS PORT Configuration Register (MBAR 0B00h) as 1010, the ETH8 is &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;UART5e_CD, the ETH15 is UART4_CTS and ETH16 is UART4_CD signals. These pins cannot be uses as GPIO for this configuration. See the Figure 2-9 of the MPC5200B User's Manual. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;You can use CD (carrier detect) signals as GPIO inputs using Input Port Change Register. See the Table 15-13 of the MPC5200B Reference Manual.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Dec 2016 11:48:33 GMT</pubDate>
    <dc:creator>Pavel</dc:creator>
    <dc:date>2016-12-29T11:48:33Z</dc:date>
    <item>
      <title>Using Ethernet port for alternate functionality</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Using-Ethernet-port-for-alternate-functionality/m-p/640501#M6292</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In mpc5200B, we have configured Ethernet port (bit 12:15) of GPS PORT Configuration Register (MBAR + 0B00h) as 1010 (i,e. Two UARTes, J1850).&lt;/P&gt;&lt;P&gt;While in this configuration,&amp;nbsp;we are not using ETH_8, ETH_15 &amp;amp; ETH_16 pins for its specified functionality&amp;nbsp;i.e,&amp;nbsp;UART5e_CD,&amp;nbsp;UART4_CTS &amp;amp;&amp;nbsp;UART4_CD respectively. Rather, we want to use these pins as GPIO, i.e, we want to read and write from/to these pins as in GPIO configuration without configuring&amp;nbsp;&lt;SPAN&gt;Ethernet port (bit 12:15) of GPS PORT Configuration Register (MBAR + 0B00h) as 0000 (i.e,&amp;nbsp;GPIO).&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please suggest us the method to achieve that?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Dec 2016 16:11:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Using-Ethernet-port-for-alternate-functionality/m-p/640501#M6292</guid>
      <dc:creator>pavangidaveer</dc:creator>
      <dc:date>2016-12-23T16:11:53Z</dc:date>
    </item>
    <item>
      <title>Re: Using Ethernet port for alternate functionality</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Using-Ethernet-port-for-alternate-functionality/m-p/640502#M6293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;If the MPC5200B Ethernet is configured using the &lt;SPAN style="color: black;"&gt;GPS PORT Configuration Register (MBAR 0B00h) as 1010, the ETH8 is &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;UART5e_CD, the ETH15 is UART4_CTS and ETH16 is UART4_CD signals. These pins cannot be uses as GPIO for this configuration. See the Figure 2-9 of the MPC5200B User's Manual. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;You can use CD (carrier detect) signals as GPIO inputs using Input Port Change Register. See the Table 15-13 of the MPC5200B Reference Manual.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Dec 2016 11:48:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Using-Ethernet-port-for-alternate-functionality/m-p/640502#M6293</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2016-12-29T11:48:33Z</dc:date>
    </item>
  </channel>
</rss>