<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: MPC5646C CSE Questions</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5646C-CSE-Questions/m-p/639112#M6252</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Yes, If MASTER_ECU_KEY is unknown, you can not launch DEBUG_AUTH command to erase the user keys.&lt;/LI&gt;&lt;LI&gt;Yes DEBUG_AUTH command erases al user keys including BOOT_MAC_KEY 3. There is no way to identify it directly but you can use the negative approach to do the same. You may perform any operation using a key and returned error should tell you whether the slot had key or was empty.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Oct 2016 07:18:43 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2016-10-13T07:18:43Z</dc:date>
    <item>
      <title>MPC5646C CSE Questions</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5646C-CSE-Questions/m-p/639111#M6251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir,&lt;/P&gt;&lt;P&gt;Some questions on MPC5646C CSE.&lt;/P&gt;&lt;P&gt;1) Because Debug Authorization command need input using KDF (MASTER_EUC_KEY, DEBUG_KEY_C)&lt;/P&gt;&lt;P&gt;If MASTER_ECU_KEY is unknown, we have no way to erase the MCU's user keys?&lt;/P&gt;&lt;P&gt;2) &lt;SPAN&gt;Debug Authorization command will erase all user keys.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Does here user key include BOOT_MAC_KEY?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3) How can we identify a key slot is empty?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;For a fresh part we need load key for the very first time.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Should we just use LOAD_KEY command directly and the error code will be returned if it's not empty?&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jason Yang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 15:59:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5646C-CSE-Questions/m-p/639111#M6251</guid>
      <dc:creator>jinjingyang</dc:creator>
      <dc:date>2016-09-21T15:59:05Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5646C CSE Questions</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5646C-CSE-Questions/m-p/639112#M6252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Yes, If MASTER_ECU_KEY is unknown, you can not launch DEBUG_AUTH command to erase the user keys.&lt;/LI&gt;&lt;LI&gt;Yes DEBUG_AUTH command erases al user keys including BOOT_MAC_KEY 3. There is no way to identify it directly but you can use the negative approach to do the same. You may perform any operation using a key and returned error should tell you whether the slot had key or was empty.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 07:18:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5646C-CSE-Questions/m-p/639112#M6252</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2016-10-13T07:18:43Z</dc:date>
    </item>
  </channel>
</rss>