<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPC5674F ：ADDR bus is 32-bit or 24-bit? in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5674F-ADDR-bus-is-32-bit-or-24-bit/m-p/636360#M6122</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello NXP:&lt;BR /&gt;I develop a firmware with MPC5674F, and have a new question about the EBI.&lt;/P&gt;&lt;P&gt;in muxed 32-bit mode(MPC5674FRM Table29-3),the address bus which is latched can be 32-bit? Or ,the available address is only 24-bit,and the A[0:7] is always 0b00000000 for ever ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 23 Apr 2017 14:05:48 GMT</pubDate>
    <dc:creator>ypchen</dc:creator>
    <dc:date>2017-04-23T14:05:48Z</dc:date>
    <item>
      <title>MPC5674F ：ADDR bus is 32-bit or 24-bit?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5674F-ADDR-bus-is-32-bit-or-24-bit/m-p/636360#M6122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello NXP:&lt;BR /&gt;I develop a firmware with MPC5674F, and have a new question about the EBI.&lt;/P&gt;&lt;P&gt;in muxed 32-bit mode(MPC5674FRM Table29-3),the address bus which is latched can be 32-bit? Or ,the available address is only 24-bit,and the A[0:7] is always 0b00000000 for ever ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Apr 2017 14:05:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5674F-ADDR-bus-is-32-bit-or-24-bit/m-p/636360#M6122</guid>
      <dc:creator>ypchen</dc:creator>
      <dc:date>2017-04-23T14:05:48Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5674F ：ADDR bus is 32-bit or 24-bit?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5674F-ADDR-bus-is-32-bit-or-24-bit/m-p/636361#M6123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, it can be 32-bit.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pay attention to section 3 in following document:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-101725"&gt;https://community.nxp.com/docs/DOC-101725&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Apr 2017 11:53:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5674F-ADDR-bus-is-32-bit-or-24-bit/m-p/636361#M6123</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2017-04-24T11:53:51Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5674F ：ADDR bus is 32-bit or 24-bit?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5674F-ADDR-bus-is-32-bit-or-24-bit/m-p/636362#M6124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,David Tosenovjan&lt;/P&gt;&lt;P&gt;My&amp;nbsp;board has two LVTH16373 to latch 32-bit Addresses.&lt;/P&gt;&lt;P&gt;But ,the&amp;nbsp;A[0:7] is always 0b00000000,and the&amp;nbsp;other 24-bit Addresses&amp;nbsp;are OK . The SIU.PCR of&amp;nbsp;D_ADD_DAT[0:15] are the same.&amp;nbsp; I want to use the upper 8 address,what can I do ?&lt;/P&gt;&lt;P&gt;Can you explain&amp;nbsp; MPC5674FRM Page 29-4.&amp;nbsp;With&amp;nbsp;this NOTE,&amp;nbsp;if Addr can be 32-bit , I think the &amp;nbsp;&lt;SPAN&gt;A[0:7] should be 0b001X_XXXX,because the&amp;nbsp;range is from 0x2000_0000&amp;nbsp;to&amp;nbsp;0x3FFF_FFFF.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="11111.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/18009i113743D3B9AA2460/image-size/large?v=v2&amp;amp;px=999" role="button" title="11111.png" alt="11111.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 May 2017 14:30:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5674F-ADDR-bus-is-32-bit-or-24-bit/m-p/636362#M6124</guid>
      <dc:creator>ypchen</dc:creator>
      <dc:date>2017-05-16T14:30:34Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5674F ：ADDR bus is 32-bit or 24-bit?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5674F-ADDR-bus-is-32-bit-or-24-bit/m-p/636363#M6125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you have set D16_31 bit?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Apr 2018 10:41:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5674F-ADDR-bus-is-32-bit-or-24-bit/m-p/636363#M6125</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2018-04-10T10:41:43Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5674F ：ADDR bus is 32-bit or 24-bit?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5674F-ADDR-bus-is-32-bit-or-24-bit/m-p/636364#M6126</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes,I set it.&lt;/P&gt;&lt;P&gt;The EBI.MCR = 0x0000_0806 .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2018 08:45:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5674F-ADDR-bus-is-32-bit-or-24-bit/m-p/636364#M6126</guid>
      <dc:creator>ypchen</dc:creator>
      <dc:date>2018-04-11T08:45:50Z</dc:date>
    </item>
  </channel>
</rss>