<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5604S priority issue in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5604S-priority-issue/m-p/632917#M5946</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CW has pre-prepared everything what is needed to handle interrupts and exceptions.&lt;BR /&gt;Generated stationery contains files Exceptions.c and IntcInterrupts.c.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These files includes required initialization and also function INTC_InstallINTCInterruptHandler that is intended to create interrupt vector table and has 3 parameters (name of the function, vector and priority).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can add function like this to your project:&lt;BR /&gt;static void Interrupts_init(void) &lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Initialize interrupts and exceptions&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; EXCEP_InitExceptionHandlers();&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; INTC_InitINTCInterrupts();&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Create interrupt vector table&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; INTC_InstallINTCInterruptHandler(handler_1,103,2);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; NTC_InstallINTCInterruptHandler(handler_2,102,1);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Lower INTC's current priority */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; INTC.CPR.B.PRI = 0;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also pay attention to interrupt nesting:&lt;BR /&gt;If INTC_NESTED_INTERRUPT == 0&lt;BR /&gt;&amp;nbsp;then interrupt handler is called directly, interrupts are disabled during ISR execution and ISR cannot be affected by interrupt with higher priority&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If INTC_NESTED_INTERRUPT == 1&lt;BR /&gt;&amp;nbsp;then interrupt handler contains necessary prolog and epilog and interrupts are enabled during prolog allowing interrupt with higher priority to be handled first&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Good luck and have a nice day.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Apr 2017 14:52:31 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2017-04-24T14:52:31Z</dc:date>
    <item>
      <title>MPC5604S priority issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5604S-priority-issue/m-p/632916#M5945</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using MPC5604S and eclipse based code warrior. I have enabled ADC and System timer using interrupt. ADC should have lowest priority and system timer should have highest priority.&lt;/P&gt;&lt;P&gt;Can anyone share me the code for the same. I need MPC5604S code only because am facing issue in priority. ADC interrupt gets called frequently than system timer interrupt. kindly guide me.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Apr 2017 15:11:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5604S-priority-issue/m-p/632916#M5945</guid>
      <dc:creator>akhilprasad</dc:creator>
      <dc:date>2017-04-21T15:11:02Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5604S priority issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5604S-priority-issue/m-p/632917#M5946</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CW has pre-prepared everything what is needed to handle interrupts and exceptions.&lt;BR /&gt;Generated stationery contains files Exceptions.c and IntcInterrupts.c.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These files includes required initialization and also function INTC_InstallINTCInterruptHandler that is intended to create interrupt vector table and has 3 parameters (name of the function, vector and priority).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can add function like this to your project:&lt;BR /&gt;static void Interrupts_init(void) &lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Initialize interrupts and exceptions&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; EXCEP_InitExceptionHandlers();&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; INTC_InitINTCInterrupts();&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Create interrupt vector table&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; INTC_InstallINTCInterruptHandler(handler_1,103,2);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; NTC_InstallINTCInterruptHandler(handler_2,102,1);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Lower INTC's current priority */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; INTC.CPR.B.PRI = 0;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also pay attention to interrupt nesting:&lt;BR /&gt;If INTC_NESTED_INTERRUPT == 0&lt;BR /&gt;&amp;nbsp;then interrupt handler is called directly, interrupts are disabled during ISR execution and ISR cannot be affected by interrupt with higher priority&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If INTC_NESTED_INTERRUPT == 1&lt;BR /&gt;&amp;nbsp;then interrupt handler contains necessary prolog and epilog and interrupts are enabled during prolog allowing interrupt with higher priority to be handled first&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Good luck and have a nice day.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Apr 2017 14:52:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5604S-priority-issue/m-p/632917#M5946</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2017-04-24T14:52:31Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5604S priority issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5604S-priority-issue/m-p/632918#M5947</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks for the input. but i can explain u what is the issue am facing. I have 3 interrupts&lt;/P&gt;&lt;P&gt;a. ADC&amp;nbsp;&amp;nbsp;&amp;nbsp;-&amp;nbsp;&amp;nbsp;&amp;nbsp;low priority&lt;/P&gt;&lt;P&gt;b. System Timer&amp;nbsp;&amp;nbsp;&amp;nbsp;- highest Priority&lt;/P&gt;&lt;P&gt;c. 2 CAN RX interrupts.&amp;nbsp;&amp;nbsp;&amp;nbsp;- medium priority&lt;/P&gt;&lt;P&gt;So during ADC initialization am&amp;nbsp;using this below code&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;INTC_InstallINTCInterruptHandler(ADC0_EOC_isr,62,2); &lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;INTC.CPR.R = 2;.&lt;/P&gt;&lt;P&gt;- During System Timer initialization &lt;SPAN&gt;am&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;using this below code&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;INTC_InstallINTCInterruptHandler(STM0_interrupt_isr,30,15);&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;INTC.CPR.R = 15;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;- During CAN&amp;nbsp;initialization &lt;SPAN&gt;am&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;using this below code&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;INTC_InstallINTCInterruptHandler(FCAN0_ReceiveInt_isr,72,9);&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;INTC.CPR.R = 15;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;INTC_InstallINTCInterruptHandler(FCAN1_ReceiveInt_isr,92,10);&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; INTC.CPR.R = 15;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;Now the issue is the interrupts are not working based on priority. ADC interrupt is continuously invoked and not allowing it to go to other interrupts.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;So I gave INTC.CPR.R in all the initialization&amp;nbsp;because from the datasheet am not clear how to use it. so can u explain me what is the relation between&amp;nbsp;&amp;nbsp;INTC.CPR.R and&amp;nbsp;INTC.PSR[vectorNum].B.PRI register. It will be great if u share me a sample code with all these functionalities I mentioned above.&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;Thanks in advance. :smileyhappy:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Apr 2017 06:33:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5604S-priority-issue/m-p/632918#M5947</guid>
      <dc:creator>akhilprasad</dc:creator>
      <dc:date>2017-04-25T06:33:30Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5604S priority issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5604S-priority-issue/m-p/632919#M5948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you tried it this way?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier,monospace;"&gt;INTC_InstallINTCInterruptHandler(ADC0_EOC_isr,62,2);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier new,courier,monospace;"&gt;INTC_InstallINTCInterruptHandler(STM0_interrupt_isr,30,15);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier new,courier,monospace;"&gt;INTC_InstallINTCInterruptHandler(FCAN0_ReceiveInt_isr,72,9);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier new,courier,monospace;"&gt;INTC_InstallINTCInterruptHandler(FCAN1_ReceiveInt_isr,92,10);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier new,courier,monospace;"&gt;INTC.CPR.R = 0;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The INTC_CPR masks any peripheral or software settable interrupt request set at the same or lower &lt;BR /&gt;priority as the current value of the INTC_CPR[PRI] field from generating an interrupt request to the &lt;BR /&gt;processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier,monospace;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Apr 2017 09:55:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5604S-priority-issue/m-p/632919#M5948</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2017-04-28T09:55:22Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5604S priority issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5604S-priority-issue/m-p/632920#M5949</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually the issues was with the CAN interrupt configuration. After re-configuring the interrupt it was working fine.&lt;/P&gt;&lt;P&gt;Thanks for the support :smileyhappy:.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Apr 2017 10:22:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5604S-priority-issue/m-p/632920#M5949</guid>
      <dc:creator>akhilprasad</dc:creator>
      <dc:date>2017-04-28T10:22:12Z</dc:date>
    </item>
  </channel>
</rss>