<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: MPC5644A DSI mode to drive TLE8718</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSI-mode-to-drive-TLE8718/m-p/631613#M5867</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Currently I don’t have any example.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This situation is being solved by using of CSI mode (combined serial interface) allowing using of DSI and SPI modes together - there is no need to switch between them.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A „data frame“ begins with “0” and this is in DSI mode automatically placed there. A „command frame“ begins with “1” and this must be send software way in SPI mode (in CSI mode no need to switch).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Nov 2016 14:31:21 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2016-11-30T14:31:21Z</dc:date>
    <item>
      <title>MPC5644A DSI mode to drive TLE8718</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSI-mode-to-drive-TLE8718/m-p/631612#M5866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to use MPC5644A to drive TLE8718, and TLE8718 requires MSC interface. So I set the DSPI on MPC5644A into DSI mode. The question is that I can not see the clock ouput and I don't know how to modify it.&lt;/P&gt;&lt;P&gt;I hope that you can provide a demo in which I can see how to configure SPI into CSI mode and to send a data .&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To drive&amp;nbsp;TLE8718, I have to send a command frame and then a data frame followed. In&amp;nbsp;the datasheet ,&amp;nbsp;I find that I can only send a data frame using DSI , and I have to change the mode to SPI if I want to send a command frame, I don't know whether I am right.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I want to send a SPI data, I know that I &amp;nbsp;just need to write data into DSPI_PUSHR. However, if I want to send a DSI data, what should I do? just write data into DSPI_ASDR?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Nov 2016 09:12:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSI-mode-to-drive-TLE8718/m-p/631612#M5866</guid>
      <dc:creator>Chenlong</dc:creator>
      <dc:date>2016-11-29T09:12:00Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5644A DSI mode to drive TLE8718</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSI-mode-to-drive-TLE8718/m-p/631613#M5867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Currently I don’t have any example.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This situation is being solved by using of CSI mode (combined serial interface) allowing using of DSI and SPI modes together - there is no need to switch between them.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A „data frame“ begins with “0” and this is in DSI mode automatically placed there. A „command frame“ begins with “1” and this must be send software way in SPI mode (in CSI mode no need to switch).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Nov 2016 14:31:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSI-mode-to-drive-TLE8718/m-p/631613#M5867</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2016-11-30T14:31:21Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5644A DSI mode to drive TLE8718</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSI-mode-to-drive-TLE8718/m-p/631614#M5868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To DSI:&lt;/P&gt;&lt;P&gt;Data may from the eTPU, eMIOS, or ASDR&lt;BR /&gt; DSPI_DSICR[TXSS] choose ASDR or SDR where SDR selects serialized eTPU or eMIOS channels.&lt;/P&gt;&lt;P&gt;These connections are described in:&lt;/P&gt;&lt;P&gt;30.9.17 DSPI connections to eTPU_A, eMIOS and SIU&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I could recommend following appnote, it describes old module version that is however backward compatible, but I think it could helpful anyway:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/assets/documents/data/en/application-notes/AN2867.pdf"&gt;http://www.nxp.com/assets/documents/data/en/application-notes/AN2867.pdf&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Nov 2016 15:44:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSI-mode-to-drive-TLE8718/m-p/631614#M5868</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2016-11-30T15:44:32Z</dc:date>
    </item>
  </channel>
</rss>