<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LIN in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/LIN/m-p/624403#M5620</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;And how to make receive function active then?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Apr 2017 09:17:00 GMT</pubDate>
    <dc:creator>monicabagade</dc:creator>
    <dc:date>2017-04-20T09:17:00Z</dc:date>
    <item>
      <title>LIN</title>
      <link>https://community.nxp.com/t5/MPC5xxx/LIN/m-p/624400#M5617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to learn &lt;STRONG&gt;LIN&lt;/STRONG&gt; functionality on &lt;STRONG&gt;MPC5634m&lt;/STRONG&gt;. In this I have tried basic transfer of single message using following code.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;#include "mpc563m.h" /* Use proper include file such as mpc5510.h or mpc5554.h */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;const uint8_t FrameSpecAndData[] = {0x35,0x08,0xD0,'H','e','l','l','o',' ',' ',' '};&amp;nbsp;&lt;BR /&gt;uint8_t&amp;nbsp; RecData;&amp;nbsp;&lt;/P&gt;&lt;P&gt;void initSysclk (void) {&lt;BR /&gt;&amp;nbsp; &amp;nbsp; FMPLL.ESYNCR1.B.CLKCFG = 0X7;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Change clk to PLL normal mode from crystal */&amp;nbsp; &lt;BR /&gt;&amp;nbsp; &amp;nbsp; FMPLL.SYNCR.R = 0x16080000;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* 8 MHz xtal: 0x16080000; 40MHz: 0x46100000 */&lt;BR /&gt;&amp;nbsp; &amp;nbsp; while (FMPLL.SYNSR.B.LOCK != 1) {}; /* Wait for FMPLL to LOCK&amp;nbsp; */&lt;BR /&gt;&amp;nbsp; &amp;nbsp; FMPLL.SYNCR.R = 0x16000000;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* 8 MHz xtal: 0x16000000; 40MHz: 0x46080000 */&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;void initESCI_B (void) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ESCI_B.CR2.R = 0x6240;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Module is enabled, 13 bit break, stop on errors */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;ESCI_B.CR1.R = 0x0180000C;&amp;nbsp; /* 10417 baud, 8 bits, no parity, Tx &amp;amp; Rx enabled */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ESCI_B.LCR.R = 0x01000000;&amp;nbsp; /* eSCI put in LIN mode */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;SIU.PCR[91].R = 0x400;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Configure pad for primary func: TxDB */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SIU.PCR[92].R = 0x400;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Configure pad for primary func: RxDB */&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;void TransmitData (void) {&lt;BR /&gt;&amp;nbsp; uint8_t&amp;nbsp;j;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Dummy variable */&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; for (j=0; j&amp;lt; sizeof (FrameSpecAndData); j++) {&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Loop for character string */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;while (ESCI_B.SR.B.TXRDY == 0) {}&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Wait for LIN transmit ready = 1 */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;ESCI_B.SR.R = 0x00004000;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Clear TXRDY flag */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;ESCI_B.LTR.R = FrameSpecAndData[j];&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Write byte to LIN Trans Reg. */&lt;BR /&gt;&amp;nbsp; }&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;void ReceiveData (void) {&lt;BR /&gt;&amp;nbsp; &amp;nbsp; while (ESCI_B.SR.B.RXRDY == 0) {}&amp;nbsp;&amp;nbsp; /* Wait for LIN transmit ready = 1 */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;ESCI_B.SR.R = 0x00008000;&amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;RecData = ESCI_B.LRR.R;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Read byte of Data*/ &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ESCI_B.LRR.R = RecData;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Echo back byte of Data read */ &lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;void main(void) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;initSysclk();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Set sysclk = 64MHz running from PLL */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;initESCI_B();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Enable Tx for 10417 baud, 8 bits, no parity */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;TransmitData();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Transmit string of characters on eSCI B */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;ReceiveData();&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while (1) {}&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Wait forever */&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;If I want to transmit multiple messages. How to do that?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Can i transfer multiple messages with same ID?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Is there any demo code with the help of DMA transfer?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me out?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Apr 2017 06:27:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/LIN/m-p/624400#M5617</guid>
      <dc:creator>monicabagade</dc:creator>
      <dc:date>2017-04-19T06:27:31Z</dc:date>
    </item>
    <item>
      <title>Re: LIN</title>
      <link>https://community.nxp.com/t5/MPC5xxx/LIN/m-p/624401#M5618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Monica,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What do you mean by multiple messages? The communication is based on single-master/multiple-slave concept. So the only Master initiates a communication by sending a header, then either transmit a data to slave or receive data from slave nodes.&lt;/P&gt;&lt;P&gt;Once the LIN Master transmit/receive full frame it can start another. Similarly as you did it in TransmitData function. The same ID can be used. Your ReceiveData function cannot work.&lt;/P&gt;&lt;P&gt;Unfortunately we do not have example which uses DMA for LIN TX/RX operation. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Apr 2017 08:42:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/LIN/m-p/624401#M5618</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-04-20T08:42:32Z</dc:date>
    </item>
    <item>
      <title>Re: LIN</title>
      <link>https://community.nxp.com/t5/MPC5xxx/LIN/m-p/624402#M5619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Petr,&lt;/P&gt;&lt;P&gt;Multiple messgaes means,&lt;/P&gt;&lt;P&gt;At the same time if i want to send the more than 1 message with different Id or same Id.&lt;/P&gt;&lt;P&gt;Like in above example HELLO (8 byte)&amp;nbsp;message is passed with Id 0x3.&lt;/P&gt;&lt;P&gt;like that if another message i want to send like HOW ARE YOU or whatever. How can I send? Can I send with same ID or different ID.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Apr 2017 09:15:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/LIN/m-p/624402#M5619</guid>
      <dc:creator>monicabagade</dc:creator>
      <dc:date>2017-04-20T09:15:45Z</dc:date>
    </item>
    <item>
      <title>Re: LIN</title>
      <link>https://community.nxp.com/t5/MPC5xxx/LIN/m-p/624403#M5620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;And how to make receive function active then?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Apr 2017 09:17:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/LIN/m-p/624403#M5620</guid>
      <dc:creator>monicabagade</dc:creator>
      <dc:date>2017-04-20T09:17:00Z</dc:date>
    </item>
    <item>
      <title>Re: LIN</title>
      <link>https://community.nxp.com/t5/MPC5xxx/LIN/m-p/624404#M5621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Monica,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At the same time just single message can be sent. After message is fully transmited or received another message can be sent again. If you need to send another ID and/or data you need to modify the code as you need.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Attached is simple example for CPU controlled LIN TX/RX frame generation tested on MPC5668G eSCI module.&lt;/P&gt;&lt;P&gt;It should be similar on MPC5634M.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Apr 2017 13:06:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/LIN/m-p/624404#M5621</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-04-20T13:06:22Z</dc:date>
    </item>
    <item>
      <title>Re: LIN</title>
      <link>https://community.nxp.com/t5/MPC5xxx/LIN/m-p/624405#M5622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Monica,&lt;/P&gt;&lt;P&gt;I used the demo same method on MPC5634M, but could not receive data normally. Could you share the code that you successfully tested?&lt;/P&gt;&lt;P&gt;Looking forward to your help.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 Apr 2020 04:08:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/LIN/m-p/624405#M5622</guid>
      <dc:creator>15870467687</dc:creator>
      <dc:date>2020-04-05T04:08:34Z</dc:date>
    </item>
  </channel>
</rss>