<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: MPC5777M PLL configuration</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5777M-PLL-configuration/m-p/623634#M5548</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MPC5777M supports a 3:2 ratio between Core clock (COMP/CHKR clock = 300 MHz) and Crossbar (fast XBAR clock = 200 MHz). So DC3 setting is correct, DC2/DC1 and DC0 should follow mentioned recommendations. You should also keep the order which is stated in Table 29-4.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BTW there is an app note dealing with CGM initialization, see &lt;A href="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4812.pdf"&gt;http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4812.pdf&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Sep 2016 08:21:01 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2016-09-19T08:21:01Z</dc:date>
    <item>
      <title>MPC5777M PLL configuration</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777M-PLL-configuration/m-p/623633#M5547</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Working on the PLL configuration, I have read in the MPC5777MRM.pdf on page 1206 that:&lt;/P&gt;&lt;P&gt;"The system clock dividers are synchronized to each other such that the rising edges of the&lt;/P&gt;&lt;P&gt;lower frequency clocks are aligned with those of the higher frequency clocks. This,&lt;/P&gt;&lt;P&gt;however, imposes limitations on the division factors which can be used. In order for the&lt;/P&gt;&lt;P&gt;synchronization to work properly, each division factor must be selected such that its&lt;/P&gt;&lt;P&gt;value is an integer multiple of each division factor that has a lower value"&lt;/P&gt;&lt;P&gt;On page 1208, it is given a correct example of configuration on table 29-4.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, I don't understand why CGM_SC_DC0[DIV] is choosen with value&amp;nbsp;3 since it is not a integer value of CGM_SC_DC3[DIV] which has a value of 2.&lt;/P&gt;&lt;P&gt;Moreover,&amp;nbsp;is the order of the configuration of these registers important ?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Paulo&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Sep 2016 12:28:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777M-PLL-configuration/m-p/623633#M5547</guid>
      <dc:creator>paulodasilvapin</dc:creator>
      <dc:date>2016-09-16T12:28:25Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777M PLL configuration</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777M-PLL-configuration/m-p/623634#M5548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MPC5777M supports a 3:2 ratio between Core clock (COMP/CHKR clock = 300 MHz) and Crossbar (fast XBAR clock = 200 MHz). So DC3 setting is correct, DC2/DC1 and DC0 should follow mentioned recommendations. You should also keep the order which is stated in Table 29-4.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BTW there is an app note dealing with CGM initialization, see &lt;A href="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4812.pdf"&gt;http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4812.pdf&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Sep 2016 08:21:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777M-PLL-configuration/m-p/623634#M5548</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2016-09-19T08:21:01Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777M PLL configuration</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777M-PLL-configuration/m-p/623635#M5549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your answer and the provided application note.&lt;/P&gt;&lt;P&gt;I have use the provided code and I have noticed that when the MC_CGM_DIV_UPD_TRIG register is written then the core registers r0 to r31 of the CPU_2 are modified to undefined values.&lt;/P&gt;&lt;P&gt;Did I miss something ?&lt;/P&gt;&lt;P&gt;Paulo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 14:09:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777M-PLL-configuration/m-p/623635#M5549</guid>
      <dc:creator>paulodasilvapin</dc:creator>
      <dc:date>2016-09-21T14:09:14Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777M PLL configuration</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777M-PLL-configuration/m-p/623636#M5550</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Another remark,&lt;/P&gt;&lt;P&gt;in the application note the field CLKCFG of &lt;SPAN lang="JA" style="font-family: HelveticaLTStd-Roman; font-size: xx-small;"&gt;&lt;SPAN lang="JA" style="font-family: HelveticaLTStd-Roman; font-size: xx-small;"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;PLLDIG_PLL0CR/&lt;SPAN lang="JA" style="font-family: HelveticaLTStd-Roman; font-size: xx-small;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;PLLDIG_PLL1CR registers&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="JA" style="font-family: HelveticaLTStd-Roman; font-size: xx-small;"&gt;&lt;SPAN lang="JA" style="font-family: HelveticaLTStd-Roman; font-size: xx-small;"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&amp;nbsp;are written but this field is marked as ReadOnly in the TRM (page 1115). I'm using T32, and I see that theses registers have a value of 0x00000100 and I can't modify them. How can I set the CLKCFG field to normal mode ?&lt;/P&gt;&lt;P&gt;Paulo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 14:33:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777M-PLL-configuration/m-p/623636#M5550</guid>
      <dc:creator>paulodasilvapin</dc:creator>
      <dc:date>2016-09-21T14:33:59Z</dc:date>
    </item>
  </channel>
</rss>