<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to program MPC5744P with MC33907 in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/How-to-program-MPC5744P-with-MC33907/m-p/622248#M5481</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use MC33097 and MPC5744P for one project. However, I fail to program MCU due to frequent resets after MC33097 is configured to normal mode. The MCU I programmed is not empty and is has bootloader and application SW. I do can program when MC33097 is configured to debug mode.&lt;BR /&gt; &lt;BR /&gt;My questions are &lt;BR /&gt;How can I program the MPC5744P when MC33097 is configured at normal mode? According to AN4766, it seems that my bootloader need to disable the watchdog refresh during INIT_FS or Normal_WD state of the fail-safe logic. But is there somebody advise me how to do so?&lt;BR /&gt;To support ISO26262, MC33097 has to be configured in normal mode. After PCB assembly, the first time the MCU is powered, the flash memory of the MCU is empty and need to be programmed. How can I program an empty MCU if MC33097 operates at normal mode? Do I need to jump MC33097 to debug mode for the first programming?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Dec 2016 03:20:32 GMT</pubDate>
    <dc:creator>xiaoguangchang</dc:creator>
    <dc:date>2016-12-19T03:20:32Z</dc:date>
    <item>
      <title>How to program MPC5744P with MC33907</title>
      <link>https://community.nxp.com/t5/MPC5xxx/How-to-program-MPC5744P-with-MC33907/m-p/622248#M5481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use MC33097 and MPC5744P for one project. However, I fail to program MCU due to frequent resets after MC33097 is configured to normal mode. The MCU I programmed is not empty and is has bootloader and application SW. I do can program when MC33097 is configured to debug mode.&lt;BR /&gt; &lt;BR /&gt;My questions are &lt;BR /&gt;How can I program the MPC5744P when MC33097 is configured at normal mode? According to AN4766, it seems that my bootloader need to disable the watchdog refresh during INIT_FS or Normal_WD state of the fail-safe logic. But is there somebody advise me how to do so?&lt;BR /&gt;To support ISO26262, MC33097 has to be configured in normal mode. After PCB assembly, the first time the MCU is powered, the flash memory of the MCU is empty and need to be programmed. How can I program an empty MCU if MC33097 operates at normal mode? Do I need to jump MC33097 to debug mode for the first programming?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Dec 2016 03:20:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/How-to-program-MPC5744P-with-MC33907/m-p/622248#M5481</guid>
      <dc:creator>xiaoguangchang</dc:creator>
      <dc:date>2016-12-19T03:20:32Z</dc:date>
    </item>
    <item>
      <title>Re: How to program MPC5744P with MC33907</title>
      <link>https://community.nxp.com/t5/MPC5xxx/How-to-program-MPC5744P-with-MC33907/m-p/622249#M5482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Already answered here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/861477"&gt;https://community.nxp.com/message/861477&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Dec 2016 13:53:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/How-to-program-MPC5744P-with-MC33907/m-p/622249#M5482</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2016-12-20T13:53:37Z</dc:date>
    </item>
  </channel>
</rss>