<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: Problem with FCCU fault injection</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Problem-with-FCCU-fault-injection/m-p/620684#M5428</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the quick reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have read the chapter 69.7 in the user manual. The mechanism of FOSU means, no matter which reaction for which error is configurated, FOSU will trigger a reset for any fault in FCCU because the 'do nothing' input from FCCU is not asserted? And this FOSU seems not to be&amp;nbsp;disabled?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I just want to get an alarm for a fault, I should stop the FOSU internal timer by doing following from FCCU according to user manual:&lt;/P&gt;&lt;P&gt;1.Reset: Long or short functional reset&lt;/P&gt;&lt;P&gt;2.IRQ: NMI or Alarm&lt;/P&gt;&lt;P&gt;3.Error out triggered (by FCCU or by SW)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The first one is clear and it is the option which I don't want. The second means the register of FCCU_NMI_EN or FCCU_IRQ_ALARM_EN can be configurated. This has been tested and it works. What is the meaning of the third option?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Jan 2017 12:51:57 GMT</pubDate>
    <dc:creator>yixinwu</dc:creator>
    <dc:date>2017-01-16T12:51:57Z</dc:date>
    <item>
      <title>Problem with FCCU fault injection</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Problem-with-FCCU-fault-injection/m-p/620682#M5426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have got a problem with FCCU fault injection.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The FCCU can be configured as the guide described. The reaction of all faults has been set as no reaction. Then I make a fault injection of NCF[7] and&amp;nbsp;no reset is done. The corresponding fault bit in NCF_S0 can be read.&amp;nbsp;It works well.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then the reaction for the fault NCF[7] has been set as short functional reset. (Only reacts if fault 7 occurs. The other faults won't trigger a reset.) I make a fault injection of NCF[7] and a reset can be observed. It works well.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The FCCU configuration remains unchanged. I make a fault injection of NCF[10] for example but a reset can also be observed. There should be no reset cause no reaction is set for NCF[10]. Why do I always get a reset, no matter which fault is injected, although no reaction has been set for this fault?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is my configuration:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="174481_174481.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/122757i50028E576EA3EBCB/image-size/large?v=v2&amp;amp;px=999" role="button" title="174481_174481.png" alt="174481_174481.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12646i6DC6F51E165781BD/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and code for fault injection:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="174483_174483.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/122758iDE39BE4ACD3E62F5/image-size/large?v=v2&amp;amp;px=999" role="button" title="174483_174483.png" alt="174483_174483.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12724i14DA62B90E52FB10/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance for help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jan 2017 10:04:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Problem-with-FCCU-fault-injection/m-p/620682#M5426</guid>
      <dc:creator>yixinwu</dc:creator>
      <dc:date>2017-01-16T10:04:06Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with FCCU fault injection</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Problem-with-FCCU-fault-injection/m-p/620683#M5427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Because your reset on NCF[10] is coming from FOSU and it is a destructive reset.&lt;/P&gt;&lt;P&gt;Not FCCU itself.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12985iE2EFABE1BC16E9D9/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;FOSU is enabled by setting any bit of NCF_E and correspondingly same bit in any of the NMI_EN, IRQ_ALARM_EN, EOUT_SIG_EN or NCFS_CFG.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jan 2017 11:32:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Problem-with-FCCU-fault-injection/m-p/620683#M5427</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-01-16T11:32:42Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with FCCU fault injection</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Problem-with-FCCU-fault-injection/m-p/620684#M5428</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the quick reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have read the chapter 69.7 in the user manual. The mechanism of FOSU means, no matter which reaction for which error is configurated, FOSU will trigger a reset for any fault in FCCU because the 'do nothing' input from FCCU is not asserted? And this FOSU seems not to be&amp;nbsp;disabled?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I just want to get an alarm for a fault, I should stop the FOSU internal timer by doing following from FCCU according to user manual:&lt;/P&gt;&lt;P&gt;1.Reset: Long or short functional reset&lt;/P&gt;&lt;P&gt;2.IRQ: NMI or Alarm&lt;/P&gt;&lt;P&gt;3.Error out triggered (by FCCU or by SW)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The first one is clear and it is the option which I don't want. The second means the register of FCCU_NMI_EN or FCCU_IRQ_ALARM_EN can be configurated. This has been tested and it works. What is the meaning of the third option?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jan 2017 12:51:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Problem-with-FCCU-fault-injection/m-p/620684#M5428</guid>
      <dc:creator>yixinwu</dc:creator>
      <dc:date>2017-01-16T12:51:57Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with FCCU fault injection</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Problem-with-FCCU-fault-injection/m-p/620685#M5429</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;It means exactly whats its name is.&lt;/P&gt;&lt;P&gt;It is a signalization via FCCU fault pins to outside world that fault has occurred.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jan 2017 13:42:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Problem-with-FCCU-fault-injection/m-p/620685#M5429</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-01-16T13:42:36Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with FCCU fault injection</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Problem-with-FCCU-fault-injection/m-p/620686#M5430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ah ok.&lt;/P&gt;&lt;P&gt;I thought the error out is always triggered by FCCU automatically. How is the case that it is not done by FCCU but by SW?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jan 2017 07:02:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Problem-with-FCCU-fault-injection/m-p/620686#M5430</guid>
      <dc:creator>yixinwu</dc:creator>
      <dc:date>2017-01-17T07:02:28Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with FCCU fault injection</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Problem-with-FCCU-fault-injection/m-p/620687#M5431</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;It means exactly what its name is.&lt;/P&gt;&lt;P&gt;SW -&amp;gt; user has to signal out fault - not done by FCCU HW.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jan 2017 14:02:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Problem-with-FCCU-fault-injection/m-p/620687#M5431</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-01-19T14:02:04Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with FCCU fault injection</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Problem-with-FCCU-fault-injection/m-p/620688#M5432</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much for the support.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jan 2017 14:49:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Problem-with-FCCU-fault-injection/m-p/620688#M5432</guid>
      <dc:creator>yixinwu</dc:creator>
      <dc:date>2017-01-19T14:49:09Z</dc:date>
    </item>
  </channel>
</rss>