<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: Watchdog timer code for MPC5674F</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Watchdog-timer-code-for-MPC5674F/m-p/393356#M540</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The default configuration of SWT is described in reference manual in Table 17-1. SWT Memory Map. In column Reset Value you can read the configuration for your SWT.&lt;/P&gt;&lt;P&gt;By default SWT is enabled and will generate a reset on a time-out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no need for sample code as the SWT is by default enabled and it is really simple.&lt;/P&gt;&lt;P&gt;If you want to configure it, then this is application specific.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One last remark:&lt;/P&gt;&lt;P&gt;If you are writing to protected SWT registers make sure you didn't forget unlock them. But this is written for every protected register:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #2873ee;"&gt;The SWT_MCR contains fields for configuring and controlling the SWT. This register is read only if either the SWT_MCR[HLK] or SWT_MCR[SLK] bits are set.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Jul 2015 07:46:59 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2015-07-08T07:46:59Z</dc:date>
    <item>
      <title>Watchdog timer code for MPC5674F</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Watchdog-timer-code-for-MPC5674F/m-p/393355#M539</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi friend,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Kindly give me the sample code for watchdog timer in&amp;nbsp; MPC5674F. And briefly explain the configurations of the watchdog timer in MPC5674F.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2015 07:19:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Watchdog-timer-code-for-MPC5674F/m-p/393355#M539</guid>
      <dc:creator>rajiilangovan</dc:creator>
      <dc:date>2015-07-08T07:19:31Z</dc:date>
    </item>
    <item>
      <title>Re: Watchdog timer code for MPC5674F</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Watchdog-timer-code-for-MPC5674F/m-p/393356#M540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The default configuration of SWT is described in reference manual in Table 17-1. SWT Memory Map. In column Reset Value you can read the configuration for your SWT.&lt;/P&gt;&lt;P&gt;By default SWT is enabled and will generate a reset on a time-out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no need for sample code as the SWT is by default enabled and it is really simple.&lt;/P&gt;&lt;P&gt;If you want to configure it, then this is application specific.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One last remark:&lt;/P&gt;&lt;P&gt;If you are writing to protected SWT registers make sure you didn't forget unlock them. But this is written for every protected register:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #2873ee;"&gt;The SWT_MCR contains fields for configuring and controlling the SWT. This register is read only if either the SWT_MCR[HLK] or SWT_MCR[SLK] bits are set.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2015 07:46:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Watchdog-timer-code-for-MPC5674F/m-p/393356#M540</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2015-07-08T07:46:59Z</dc:date>
    </item>
  </channel>
</rss>