<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: MCP5643L SWG Setting</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MCP5643L-SWG-Setting/m-p/617082#M5273</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SWG output is on the pin D[7]. On the MPC5643L EVB this pin is connected to LED4, which causes high load for the SWG output. Disconnect the LED4 (jumper J8.4) to get full swing of the SWG output.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Mar 2017 10:14:45 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2017-03-27T10:14:45Z</dc:date>
    <item>
      <title>MCP5643L SWG Setting</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MCP5643L-SWG-Setting/m-p/617081#M5272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the motor control toolbox to configure a MCP5643 eval board to generate sine wave with SWG module, but the output is not as expected: output is only about half the set value. I attached the setting and output waveform here. Can someone take a look and let me know what went wrong?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Photo Mar 24, 10 49 27 AM.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/15767i6F10DACCFFE827F3/image-size/large?v=v2&amp;amp;px=999" role="button" title="Photo Mar 24, 10 49 27 AM.jpg" alt="Photo Mar 24, 10 49 27 AM.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="SWG Output when set to 2.264V.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/15728iCC36B3A87EE00657/image-size/large?v=v2&amp;amp;px=999" role="button" title="SWG Output when set to 2.264V.jpg" alt="SWG Output when set to 2.264V.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Mar 2017 17:59:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MCP5643L-SWG-Setting/m-p/617081#M5272</guid>
      <dc:creator>jinzhuli</dc:creator>
      <dc:date>2017-03-24T17:59:45Z</dc:date>
    </item>
    <item>
      <title>Re: MCP5643L SWG Setting</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MCP5643L-SWG-Setting/m-p/617082#M5273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SWG output is on the pin D[7]. On the MPC5643L EVB this pin is connected to LED4, which causes high load for the SWG output. Disconnect the LED4 (jumper J8.4) to get full swing of the SWG output.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Mar 2017 10:14:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MCP5643L-SWG-Setting/m-p/617082#M5273</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-03-27T10:14:45Z</dc:date>
    </item>
  </channel>
</rss>