<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 CodeWarrior 10.6 Erase Flash Config</title>
    <link>https://community.nxp.com/t5/MPC5xxx/CodeWarrior-10-6-Erase-Flash-Config/m-p/615389#M5178</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Customer is using CW10.6 to develop MPC5606B software.&lt;/P&gt;&lt;P&gt;By default, when we launch the debugger, it will erase all flash and program the elf into MCU.&lt;/P&gt;&lt;P&gt;Can we modify some configurations to make it erase only the specified area of flash and program elf file?&lt;/P&gt;&lt;P&gt;(For example, customer want to keep the bootloader area from 0x00000000~0x00010000 unchanged, and erase/program the flash area after 0x00010000.)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jason Yang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Jan 2017 09:01:10 GMT</pubDate>
    <dc:creator>jinjingyang</dc:creator>
    <dc:date>2017-01-13T09:01:10Z</dc:date>
    <item>
      <title>CodeWarrior 10.6 Erase Flash Config</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CodeWarrior-10-6-Erase-Flash-Config/m-p/615389#M5178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Customer is using CW10.6 to develop MPC5606B software.&lt;/P&gt;&lt;P&gt;By default, when we launch the debugger, it will erase all flash and program the elf into MCU.&lt;/P&gt;&lt;P&gt;Can we modify some configurations to make it erase only the specified area of flash and program elf file?&lt;/P&gt;&lt;P&gt;(For example, customer want to keep the bootloader area from 0x00000000~0x00010000 unchanged, and erase/program the flash area after 0x00010000.)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jason Yang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jan 2017 09:01:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CodeWarrior-10-6-Erase-Flash-Config/m-p/615389#M5178</guid>
      <dc:creator>jinjingyang</dc:creator>
      <dc:date>2017-01-13T09:01:10Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior 10.6 Erase Flash Config</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CodeWarrior-10-6-Erase-Flash-Config/m-p/615390#M5179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jason,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, there is a feature, which allows to keep some content of flash memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Open Debug configuration of your project (flash target) and click Edit&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11895i286301EB2E3DF51E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Choose Advanced Programming Options&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11949iA06024B9EC47B517/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Choose the memory range you do not want to erase during programming.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11993i44F15620031CC524/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jan 2017 11:49:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CodeWarrior-10-6-Erase-Flash-Config/m-p/615390#M5179</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2017-01-13T11:49:37Z</dc:date>
    </item>
  </channel>
</rss>