<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PROBLEM IN FLEXCAN FD TX  in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/PROBLEM-IN-FLEXCAN-FD-TX/m-p/613109#M5070</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PS: the expression is :&lt;/P&gt;&lt;P&gt;Failed to execute MI command:&lt;/P&gt;&lt;P&gt;-data-evaluate-expression (CAN_1.FDCTRL).MBDSR0&lt;/P&gt;&lt;P&gt;Error message from debugger back end:&lt;/P&gt;&lt;P&gt;There is no member named MBDSR0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But i have found in MPC5748.h, &amp;nbsp;the example project has this definition(&lt;SPAN&gt; MBDSR0&lt;/SPAN&gt;).&lt;/P&gt;&lt;P&gt;i think something set wrong with the registers which i pay no attention to,could anyone help me?&amp;nbsp;Thanks a lot!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Dec 2016 13:24:07 GMT</pubDate>
    <dc:creator>383076174</dc:creator>
    <dc:date>2016-12-15T13:24:07Z</dc:date>
    <item>
      <title>PROBLEM IN FLEXCAN FD TX</title>
      <link>https://community.nxp.com/t5/MPC5xxx/PROBLEM-IN-FLEXCAN-FD-TX/m-p/613108#M5069</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi, i use the mpc5748 devkit to do some research on CAN FD via S32DS.&lt;/P&gt;&lt;P&gt;i have tried to configure the fd registers and got some problems when debugging.&lt;/P&gt;&lt;P&gt;i import the can0 transmit example &amp;nbsp; anmake changes on it :use can1 port,add fd function.&lt;/P&gt;&lt;P&gt;then the related codes as,followed:&lt;/P&gt;&lt;P&gt;CAN_1.MCR.B.MIDS=1;&lt;/P&gt;&lt;P&gt;CAN_1.CTRL1.B.CLKSRC=0;&lt;/P&gt;&lt;P&gt;CAN_1.MCR.B.MIDS=0;&lt;/P&gt;&lt;P&gt;WHILE(!CAN_1.MCR.BFRZACK)&lt;/P&gt;&lt;P&gt;{}&lt;/P&gt;&lt;P&gt;CAN_1.CTRL1.R=0X04DB0086;&lt;/P&gt;&lt;P&gt;//ADD BY ME&lt;/P&gt;&lt;P&gt;CAN_1MCR.B.FDEN=1;&lt;/P&gt;&lt;P&gt;CAN_1.FDCTRL.B.MBDSR0=3;&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;CAN_1.FDCBT.R=0X00431863;//500bps&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;//CODE END&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When i try to debug the project and have a sigle steP the code "CAN_1.FDCTRL...", the mistake happens and the related infomation is in the following accessory.&lt;/P&gt;&lt;P&gt;i cannot find the reason, and will appreciate if anyone sall help me,than you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 04:31:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/PROBLEM-IN-FLEXCAN-FD-TX/m-p/613108#M5069</guid>
      <dc:creator>383076174</dc:creator>
      <dc:date>2016-12-15T04:31:28Z</dc:date>
    </item>
    <item>
      <title>Re: PROBLEM IN FLEXCAN FD TX</title>
      <link>https://community.nxp.com/t5/MPC5xxx/PROBLEM-IN-FLEXCAN-FD-TX/m-p/613109#M5070</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PS: the expression is :&lt;/P&gt;&lt;P&gt;Failed to execute MI command:&lt;/P&gt;&lt;P&gt;-data-evaluate-expression (CAN_1.FDCTRL).MBDSR0&lt;/P&gt;&lt;P&gt;Error message from debugger back end:&lt;/P&gt;&lt;P&gt;There is no member named MBDSR0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But i have found in MPC5748.h, &amp;nbsp;the example project has this definition(&lt;SPAN&gt; MBDSR0&lt;/SPAN&gt;).&lt;/P&gt;&lt;P&gt;i think something set wrong with the registers which i pay no attention to,could anyone help me?&amp;nbsp;Thanks a lot!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 13:24:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/PROBLEM-IN-FLEXCAN-FD-TX/m-p/613109#M5070</guid>
      <dc:creator>383076174</dc:creator>
      <dc:date>2016-12-15T13:24:07Z</dc:date>
    </item>
    <item>
      <title>Re: PROBLEM IN FLEXCAN FD TX</title>
      <link>https://community.nxp.com/t5/MPC5xxx/PROBLEM-IN-FLEXCAN-FD-TX/m-p/613110#M5071</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mandy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you please send us the whole project so we can test your issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Dec 2016 09:39:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/PROBLEM-IN-FLEXCAN-FD-TX/m-p/613110#M5071</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2016-12-20T09:39:55Z</dc:date>
    </item>
  </channel>
</rss>