<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: MPC5744P  about PMC</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-about-PMC/m-p/612269#M5036</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You can invoke the fault by injecting it via PMC module.&lt;/P&gt;&lt;P&gt;Then you must see the faults reported in FCCU.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10886iAEBEEC4AE4A3F978/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I suppose there is no SW example needed as this is very simple.&lt;/P&gt;&lt;P&gt;Just inject the fault via PMC and verify if the fault was latched in FCCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Dec 2016 07:54:33 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2016-12-15T07:54:33Z</dc:date>
    <item>
      <title>MPC5744P  about PMC</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-about-PMC/m-p/612268#M5035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;UL&gt;&lt;LI&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Safety Manual for MPC5744P&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Assumption&lt;/STRONG&gt;: [SM_144] The application software must initiate the hardware-assisted&lt;BR /&gt;self-test to detect LVD/HVD failures after startup. [end]&lt;BR /&gt;&lt;STRONG&gt;Assumption&lt;/STRONG&gt;: [SM_084] The application software must check the status registers of the&lt;BR /&gt;FCCU and MC_RGM for the results of the hardware-assisted self-test. [end]&lt;/LI&gt;&lt;/UL&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; how we can detect LVD/HVD ?&amp;nbsp; can you give our some software example about how te detect LVD/HVD ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 02:32:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P-about-PMC/m-p/612268#M5035</guid>
      <dc:creator>xiaobozheng</dc:creator>
      <dc:date>2016-12-15T02:32:27Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P  about PMC</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-about-PMC/m-p/612269#M5036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You can invoke the fault by injecting it via PMC module.&lt;/P&gt;&lt;P&gt;Then you must see the faults reported in FCCU.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10886iAEBEEC4AE4A3F978/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I suppose there is no SW example needed as this is very simple.&lt;/P&gt;&lt;P&gt;Just inject the fault via PMC and verify if the fault was latched in FCCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 07:54:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P-about-PMC/m-p/612269#M5036</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2016-12-15T07:54:33Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P  about PMC</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-about-PMC/m-p/612270#M5037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Assumption: [SM_204] It is assumed that the ADC's are used to monitor the bandgap&lt;BR /&gt;reference voltage of the PMC. [end]&lt;BR /&gt;Apart from the self-test and ADC monitoring of the bandgap reference voltage, the use of&lt;BR /&gt;the PMC for safety-relevant applications is transparent to the user.&lt;BR /&gt;&lt;STRONG&gt;The PMC BISTs are automatically run during startup, but the LVDs and HVDs are&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;disabled until after testing completes.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;as your means,if testing completes,&amp;nbsp;the LVDs and HVDs will be automatically running? we&amp;nbsp; do not need to do anything, just need to check FCCU? &lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Dec 2016 02:11:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P-about-PMC/m-p/612270#M5037</guid>
      <dc:creator>xiaobozheng</dc:creator>
      <dc:date>2016-12-16T02:11:01Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P  about PMC</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-about-PMC/m-p/612271#M5038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The LVD/HVD is running except PMC BIST.&lt;/P&gt;&lt;P&gt;What you have to do is to test is PMC can react on LVD/HVD violation by injecting the fault to PMC and checking reaction path up to FCCU.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Dec 2016 08:10:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P-about-PMC/m-p/612271#M5038</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2016-12-16T08:10:32Z</dc:date>
    </item>
  </channel>
</rss>