<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: PWM frequency for MPC5646</title>
    <link>https://community.nxp.com/t5/MPC5xxx/PWM-frequency-for-MPC5646/m-p/158226#M5</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you mean eMIOS PWM then eMIOS belongs to peripheral set 3 which can be clocked by frequency derived (divide from /1 to /16 (CGM_SC_DC2 Register)) from sysclk (max 120MHz). Next divider in series to previous is a global prescaler of eMIOS module (1~256). So, max input clock for PWM can be pwmclk = 120/1/1=120MHz. Now the period of the PWM signal is defined by PWM period setup for defined mode. fPWM = period / pwmclk.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards, Ladislav&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 Oct 2012 06:09:48 GMT</pubDate>
    <dc:creator>lama</dc:creator>
    <dc:date>2012-10-31T06:09:48Z</dc:date>
    <item>
      <title>PWM frequency for MPC5646</title>
      <link>https://community.nxp.com/t5/MPC5xxx/PWM-frequency-for-MPC5646/m-p/158225#M4</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I read in an application note, that PWM frequencies are usually between 1KHz and 100KHz. But I also read in the DS of the MPC5646 that the peripheral frequency is in the range 8MHz-120MHz.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So what is exactly the frequency of the PWM module for the MPC5646? I need a high frequency like the peripheral frequency (more than 8MHz), is that possible?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Oct 2012 15:28:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/PWM-frequency-for-MPC5646/m-p/158225#M4</guid>
      <dc:creator>phobos973</dc:creator>
      <dc:date>2012-10-30T15:28:41Z</dc:date>
    </item>
    <item>
      <title>Re: PWM frequency for MPC5646</title>
      <link>https://community.nxp.com/t5/MPC5xxx/PWM-frequency-for-MPC5646/m-p/158226#M5</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you mean eMIOS PWM then eMIOS belongs to peripheral set 3 which can be clocked by frequency derived (divide from /1 to /16 (CGM_SC_DC2 Register)) from sysclk (max 120MHz). Next divider in series to previous is a global prescaler of eMIOS module (1~256). So, max input clock for PWM can be pwmclk = 120/1/1=120MHz. Now the period of the PWM signal is defined by PWM period setup for defined mode. fPWM = period / pwmclk.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards, Ladislav&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Oct 2012 06:09:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/PWM-frequency-for-MPC5646/m-p/158226#M5</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2012-10-31T06:09:48Z</dc:date>
    </item>
  </channel>
</rss>