<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CW2.10,SPC5605b auto connect problem? in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/CW2-10-SPC5605b-auto-connect-problem/m-p/610302#M4959</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;CW2.10,My design use SPC5605bmll6,When debuging,if CPU setting is autodetect,in high level load dialog, Program binary image into Flash using default Algorithm for Selected Device is MPC5606BK(Autodetect).&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; If CPU setting is MPC5605B,in high level load dialog, Program binary image into Flash using default Algorithm for Selected Device is MPC5606B.While I Add Register in Variables window,it is all MPC5607B register.&lt;/P&gt;&lt;P&gt;&amp;nbsp; 1. &amp;nbsp;I what to know that is OK or not.&lt;/P&gt;&lt;P&gt;&amp;nbsp; 2.At the same time,In project I cannot change all PCR.R.but In memory window,I can write data in sram(0x40000000).and ex-clock is OK.&lt;/P&gt;&lt;P&gt;need help&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;THANKS&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Mar 2017 07:39:03 GMT</pubDate>
    <dc:creator>wuxuliang</dc:creator>
    <dc:date>2017-03-01T07:39:03Z</dc:date>
    <item>
      <title>CW2.10,SPC5605b auto connect problem?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CW2-10-SPC5605b-auto-connect-problem/m-p/610302#M4959</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;CW2.10,My design use SPC5605bmll6,When debuging,if CPU setting is autodetect,in high level load dialog, Program binary image into Flash using default Algorithm for Selected Device is MPC5606BK(Autodetect).&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; If CPU setting is MPC5605B,in high level load dialog, Program binary image into Flash using default Algorithm for Selected Device is MPC5606B.While I Add Register in Variables window,it is all MPC5607B register.&lt;/P&gt;&lt;P&gt;&amp;nbsp; 1. &amp;nbsp;I what to know that is OK or not.&lt;/P&gt;&lt;P&gt;&amp;nbsp; 2.At the same time,In project I cannot change all PCR.R.but In memory window,I can write data in sram(0x40000000).and ex-clock is OK.&lt;/P&gt;&lt;P&gt;need help&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;THANKS&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Mar 2017 07:39:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CW2-10-SPC5605b-auto-connect-problem/m-p/610302#M4959</guid>
      <dc:creator>wuxuliang</dc:creator>
      <dc:date>2017-03-01T07:39:03Z</dc:date>
    </item>
    <item>
      <title>Re: CW2.10,SPC5605b auto connect problem?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CW2-10-SPC5605b-auto-connect-problem/m-p/610303#M4960</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what do you mean by:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Program binary image into Flash using default Algorithm for Selected Device is MPC5606BK(Autodetect).&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;&amp;nbsp; &amp;nbsp; If CPU setting is MPC5605B,in high level load dialog, Program binary image into Flash using default Algorithm for Selected Device is MPC5606B&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where did you check that this algorithm was used?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About your second question, please read my answer in your second thread:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/445957"&gt;https://community.nxp.com/thread/445957&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Mar 2017 15:20:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CW2-10-SPC5605b-auto-connect-problem/m-p/610303#M4960</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2017-03-02T15:20:13Z</dc:date>
    </item>
  </channel>
</rss>