<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: The Flash memory ECC failure reporting path check</title>
    <link>https://community.nxp.com/t5/MPC5xxx/The-Flash-memory-ECC-failure-reporting-path-check/m-p/608462#M4886</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not exactly. It is not needed to write any data to UTEST region, they are already pre-prepared there from factory (moreover UTEST region is one-time-programmable and already programmed).&lt;/P&gt;&lt;P&gt;I have just prepared example code here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-333754"&gt;https://community.nxp.com/docs/DOC-333754&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Jan 2017 08:31:54 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2017-01-13T08:31:54Z</dc:date>
    <item>
      <title>The Flash memory ECC failure reporting path check</title>
      <link>https://community.nxp.com/t5/MPC5xxx/The-Flash-memory-ECC-failure-reporting-path-check/m-p/608461#M4885</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Assumption: [SM_119] The Flash memory ECC failure reporting path should be&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;checked to validate if detected ECC faults are correctly reported.&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Implementation hint: The flash memory ECC fault report check is executed in&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;software . The test consists of software reading from the flash memory UTest area (see&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;"UTEST flash memory map" table in the "Memory map" chapter of the MPC5744P&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Reference Manual). a set of test patterns to test the integrity of the ECC logic fault&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;reporting path to the MEMU and FCCU (executed at start-up, latent failure measure).&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;question:&amp;nbsp;&amp;nbsp; is this means:&amp;nbsp; we can write some data into utest &amp;nbsp;region (0x00400040-0x00400060), rading it back and check the fccu or memu flag ? &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp; if this is not right, please tell me how can i check flash ecc failure report path,&amp;nbsp; thanks !&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jan 2017 07:35:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/The-Flash-memory-ECC-failure-reporting-path-check/m-p/608461#M4885</guid>
      <dc:creator>xiaobozheng</dc:creator>
      <dc:date>2017-01-12T07:35:38Z</dc:date>
    </item>
    <item>
      <title>Re: The Flash memory ECC failure reporting path check</title>
      <link>https://community.nxp.com/t5/MPC5xxx/The-Flash-memory-ECC-failure-reporting-path-check/m-p/608462#M4886</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not exactly. It is not needed to write any data to UTEST region, they are already pre-prepared there from factory (moreover UTEST region is one-time-programmable and already programmed).&lt;/P&gt;&lt;P&gt;I have just prepared example code here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-333754"&gt;https://community.nxp.com/docs/DOC-333754&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jan 2017 08:31:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/The-Flash-memory-ECC-failure-reporting-path-check/m-p/608462#M4886</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2017-01-13T08:31:54Z</dc:date>
    </item>
  </channel>
</rss>