<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: MPC5643l capture problem</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5643l-capture-problem/m-p/608139#M4865</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Look at Figure 25-26 and description in the “E-Capture” chapter within a Reference Manual.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When INPSELX=0 then the PWMX input signal goes directly to both Capture circuits. By the EDGX1/EDGX0 bits you can select at which signal edge the internal counter value will be captured.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When INPSELX=1 then the input signal comes to an 8 bit counter which counts both the rising and falling edges.&amp;nbsp; The output of this counter is compared to an 8 bit value that is specified by the user (EDGCMPx) and when the two values are equal, the comparator generates a pulse that also resets the 8bit counter.&amp;nbsp; This output pulse is then used to trigger capture logic. Note: EDGX1/EDGX0 bits must be set still to enable capture logic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Nov 2016 08:55:32 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2016-11-21T08:55:32Z</dc:date>
    <item>
      <title>MPC5643l capture problem</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5643l-capture-problem/m-p/608138#M4864</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/122536i1627E4E26A9434E7/image-size/large?v=v2&amp;amp;px=999" title="169976_169976.PNG" alt="169976_169976.PNG" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/8715iEAD3CB52051625CC/image-size/large?v=v2&amp;amp;px=999" title="捕获.PNG" alt="捕获.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This is one bit in flexPWM module about the register of &amp;nbsp;Capture Control X Register (CAPTCTRLX). I can not understand the mean of &amp;nbsp;the different between 1and 0 and how to use them. I need &amp;nbsp;the help of an expert.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much for your help&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 20 Nov 2016 12:59:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5643l-capture-problem/m-p/608138#M4864</guid>
      <dc:creator>zcc890406</dc:creator>
      <dc:date>2016-11-20T12:59:20Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5643l capture problem</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5643l-capture-problem/m-p/608139#M4865</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Look at Figure 25-26 and description in the “E-Capture” chapter within a Reference Manual.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When INPSELX=0 then the PWMX input signal goes directly to both Capture circuits. By the EDGX1/EDGX0 bits you can select at which signal edge the internal counter value will be captured.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When INPSELX=1 then the input signal comes to an 8 bit counter which counts both the rising and falling edges.&amp;nbsp; The output of this counter is compared to an 8 bit value that is specified by the user (EDGCMPx) and when the two values are equal, the comparator generates a pulse that also resets the 8bit counter.&amp;nbsp; This output pulse is then used to trigger capture logic. Note: EDGX1/EDGX0 bits must be set still to enable capture logic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Nov 2016 08:55:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5643l-capture-problem/m-p/608139#M4865</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2016-11-21T08:55:32Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5643l capture problem</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5643l-capture-problem/m-p/608140#M4866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Petr Stancik,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Thank you for your help.&amp;nbsp;&amp;nbsp;Now I understand how to use it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tomas.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Nov 2016 12:34:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5643l-capture-problem/m-p/608140#M4866</guid>
      <dc:creator>zcc890406</dc:creator>
      <dc:date>2016-11-21T12:34:30Z</dc:date>
    </item>
  </channel>
</rss>