<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TSENS MPC5675K in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/TSENS-MPC5675K/m-p/606344#M4804</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have just tried it (with MPC5643L but it should be the same) and I can also see mentioned temperature shift in case 5V is used instead of 3.3V. I am investigating details, letting you know then…&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Sep 2016 14:29:22 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2016-09-12T14:29:22Z</dc:date>
    <item>
      <title>TSENS MPC5675K</title>
      <link>https://community.nxp.com/t5/MPC5xxx/TSENS-MPC5675K/m-p/606343#M4803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are seeing a processor temperature on the TSENS of the MPC5675K that is consistently +10 deg C above the temperature read on the thermal scan. &amp;nbsp;Why is that?&lt;/P&gt;&lt;P&gt;One point about our design is that the ADC reference voltage is 5 V instead of 3.3.&lt;/P&gt;&lt;P&gt;We expect a 12-bit resolution, so I'm masking off the most significant 4 bits of the calibration values.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Sep 2016 17:24:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/TSENS-MPC5675K/m-p/606343#M4803</guid>
      <dc:creator>laurayindra</dc:creator>
      <dc:date>2016-09-09T17:24:25Z</dc:date>
    </item>
    <item>
      <title>Re: TSENS MPC5675K</title>
      <link>https://community.nxp.com/t5/MPC5xxx/TSENS-MPC5675K/m-p/606344#M4804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have just tried it (with MPC5643L but it should be the same) and I can also see mentioned temperature shift in case 5V is used instead of 3.3V. I am investigating details, letting you know then…&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Sep 2016 14:29:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/TSENS-MPC5675K/m-p/606344#M4804</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2016-09-12T14:29:22Z</dc:date>
    </item>
    <item>
      <title>Re: TSENS MPC5675K</title>
      <link>https://community.nxp.com/t5/MPC5xxx/TSENS-MPC5675K/m-p/606345#M4805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been confirmed that ADC reference does not affect accuracy of temperature sensor. Even though it is a bit different it should be still in specified tolerance +/-10°C. Note that this sensor is relatively imprecise.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Sep 2016 12:30:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/TSENS-MPC5675K/m-p/606345#M4805</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2016-09-20T12:30:29Z</dc:date>
    </item>
    <item>
      <title>Re: TSENS MPC5675K</title>
      <link>https://community.nxp.com/t5/MPC5xxx/TSENS-MPC5675K/m-p/606346#M4806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with Laura on the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;MPC5675K temperature sensor issue. &amp;nbsp;We are consistently seeing the calculated value of the sensor to be +18 to +20 degrees C above the case temperature. &amp;nbsp;This is outside the specified +/-10 C tolerance.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;What is the recommended method to account for the 5 vdc reference in the TSENS calculation?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Sep 2016 16:21:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/TSENS-MPC5675K/m-p/606346#M4806</guid>
      <dc:creator>wittkop</dc:creator>
      <dc:date>2016-09-20T16:21:44Z</dc:date>
    </item>
  </channel>
</rss>