<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic problem while using Chip select pin along with a GPIO pin in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/problem-while-using-Chip-select-pin-along-with-a-GPIO-pin/m-p/605858#M4770</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using MPC5200B as master in our device.&lt;/P&gt;&lt;P&gt;While using Chip Select 1, we have observed that we are not able to assert PSC6_3 (configured as GPIO) while chip select is kept asserted. &lt;BR /&gt;That is, even if we extend wait period of Chip Select 1 and assert PSC6_3 in the next instruction itself, actual assertion occurs only after chip select gets de-asserted.&lt;BR /&gt;In our application we needed to assert PSC6_3 while keeping Chip Select asserted. &lt;BR /&gt;Could you please tell us why this unexpected delay is occuring?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Pavan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Feb 2017 07:52:08 GMT</pubDate>
    <dc:creator>pavangidaveer</dc:creator>
    <dc:date>2017-02-06T07:52:08Z</dc:date>
    <item>
      <title>problem while using Chip select pin along with a GPIO pin</title>
      <link>https://community.nxp.com/t5/MPC5xxx/problem-while-using-Chip-select-pin-along-with-a-GPIO-pin/m-p/605858#M4770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using MPC5200B as master in our device.&lt;/P&gt;&lt;P&gt;While using Chip Select 1, we have observed that we are not able to assert PSC6_3 (configured as GPIO) while chip select is kept asserted. &lt;BR /&gt;That is, even if we extend wait period of Chip Select 1 and assert PSC6_3 in the next instruction itself, actual assertion occurs only after chip select gets de-asserted.&lt;BR /&gt;In our application we needed to assert PSC6_3 while keeping Chip Select asserted. &lt;BR /&gt;Could you please tell us why this unexpected delay is occuring?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Pavan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2017 07:52:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/problem-while-using-Chip-select-pin-along-with-a-GPIO-pin/m-p/605858#M4770</guid>
      <dc:creator>pavangidaveer</dc:creator>
      <dc:date>2017-02-06T07:52:08Z</dc:date>
    </item>
    <item>
      <title>Re: problem while using Chip select pin along with a GPIO pin</title>
      <link>https://community.nxp.com/t5/MPC5xxx/problem-while-using-Chip-select-pin-along-with-a-GPIO-pin/m-p/605859#M4771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;The MPC5200B Chip Select pins and PSC6 pins are independent pins. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;See the Table 2-24 of the MPC5200B Reference Manual.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;Perhaps there is unexpected short-circuit between the Chip Select 1 and PSC6_3. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;Check your board about unexpected short-circuit between the Chip Select 1 and PSC6_3.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Feb 2017 11:43:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/problem-while-using-Chip-select-pin-along-with-a-GPIO-pin/m-p/605859#M4771</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2017-02-08T11:43:04Z</dc:date>
    </item>
  </channel>
</rss>