<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: Calypso 3M EEPROM emulation</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Calypso-3M-EEPROM-emulation/m-p/604689#M4698</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Neo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm afraid that currently there's no such example. It will be necessary to write own definition of EE blocks in ee_block.h because it is different against other devices. There are examples for MPC5744P, MPC5746R, MPC5775K - all of them have data flash at address 0x80_0000. Then there's MPC5777C which has four 64KB block at address 0x0 (example is included in the package too) and MPC5748G/MPC5746C where you can use up to eight 16KB blocks at 0x00F9_0000.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Jan 2017 12:16:29 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2017-01-12T12:16:29Z</dc:date>
    <item>
      <title>Calypso 3M EEPROM emulation</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Calypso-3M-EEPROM-emulation/m-p/604688#M4697</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello team,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do we have EEPROM emulation driver demo project for Calypso 3M?&lt;/P&gt;&lt;P&gt;Currently driver demo does not have Calypso family's project.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Neo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jan 2017 08:07:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Calypso-3M-EEPROM-emulation/m-p/604688#M4697</guid>
      <dc:creator>neojung</dc:creator>
      <dc:date>2017-01-11T08:07:32Z</dc:date>
    </item>
    <item>
      <title>Re: Calypso 3M EEPROM emulation</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Calypso-3M-EEPROM-emulation/m-p/604689#M4698</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Neo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm afraid that currently there's no such example. It will be necessary to write own definition of EE blocks in ee_block.h because it is different against other devices. There are examples for MPC5744P, MPC5746R, MPC5775K - all of them have data flash at address 0x80_0000. Then there's MPC5777C which has four 64KB block at address 0x0 (example is included in the package too) and MPC5748G/MPC5746C where you can use up to eight 16KB blocks at 0x00F9_0000.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jan 2017 12:16:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Calypso-3M-EEPROM-emulation/m-p/604689#M4698</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2017-01-12T12:16:29Z</dc:date>
    </item>
  </channel>
</rss>