<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Need sample code MPC5777M Fast Ethernet Controller to communicate TJA1100 NXP  PHY</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Need-sample-code-MPC5777M-Fast-Ethernet-Controller-to/m-p/604194#M4673</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;We are using MPC5777M Controller in our project. I have to communicate with Ethernet Controller with TJA1100 (OPEN Alliance Broad R-Reach PHY for Automotive Ethernet). I need sample code, Application Note &amp;nbsp;for Fast Ethernet controller and guidelines for that.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Feb 2017 11:14:33 GMT</pubDate>
    <dc:creator>chidambaramvelu</dc:creator>
    <dc:date>2017-02-28T11:14:33Z</dc:date>
    <item>
      <title>Need sample code MPC5777M Fast Ethernet Controller to communicate TJA1100 NXP  PHY</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Need-sample-code-MPC5777M-Fast-Ethernet-Controller-to/m-p/604194#M4673</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;We are using MPC5777M Controller in our project. I have to communicate with Ethernet Controller with TJA1100 (OPEN Alliance Broad R-Reach PHY for Automotive Ethernet). I need sample code, Application Note &amp;nbsp;for Fast Ethernet controller and guidelines for that.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Feb 2017 11:14:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Need-sample-code-MPC5777M-Fast-Ethernet-Controller-to/m-p/604194#M4673</guid>
      <dc:creator>chidambaramvelu</dc:creator>
      <dc:date>2017-02-28T11:14:33Z</dc:date>
    </item>
    <item>
      <title>Re: Need sample code MPC5777M Fast Ethernet Controller to communicate TJA1100 NXP  PHY</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Need-sample-code-MPC5777M-Fast-Ethernet-Controller-to/m-p/604195#M4674</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a app note &lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4577.pdf?fsrch=1&amp;amp;sr=1"&gt;&lt;SPAN style="color: windowtext; text-decoration: none;"&gt;AN4577 : Using the Fast Ethernet Controller on the Qorivva MPC564xB/C&lt;/SPAN&gt;&lt;/A&gt; (&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4577.pdf"&gt;&lt;SPAN style="color: windowtext; text-decoration: none;"&gt;&lt;/SPAN&gt;&lt;/A&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4577.pdf" target="test_blank"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4577.pdf&lt;/A&gt;) with the software example. The FEC module is the same.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Attached is the AN4577 example 1 ported to the MPC5777M EVB board. You can test it directly if upi have the EVB.&lt;/P&gt;&lt;P&gt;There is DP83848c PHY, but I think it will be very similar.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Feb 2017 14:23:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Need-sample-code-MPC5777M-Fast-Ethernet-Controller-to/m-p/604195#M4674</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-02-28T14:23:25Z</dc:date>
    </item>
  </channel>
</rss>