<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックCAN with internal IRC</title>
    <link>https://community.nxp.com/t5/MPC5xxx/CAN-with-internal-IRC/m-p/603787#M4641</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have configured a CAN with peripheral clock. And the system is running with 16MHZ IRC.&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The CAN communication is not seems to be consistent. Most of the time it works but&amp;nbsp;sometime its struct with error ISR of CAN.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you give your view on this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Nov 2016 14:58:12 GMT</pubDate>
    <dc:creator>keerthidhanapal</dc:creator>
    <dc:date>2016-11-17T14:58:12Z</dc:date>
    <item>
      <title>CAN with internal IRC</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CAN-with-internal-IRC/m-p/603787#M4641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have configured a CAN with peripheral clock. And the system is running with 16MHZ IRC.&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The CAN communication is not seems to be consistent. Most of the time it works but&amp;nbsp;sometime its struct with error ISR of CAN.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you give your view on this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Nov 2016 14:58:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CAN-with-internal-IRC/m-p/603787#M4641</guid>
      <dc:creator>keerthidhanapal</dc:creator>
      <dc:date>2016-11-17T14:58:12Z</dc:date>
    </item>
    <item>
      <title>Re: CAN with internal IRC</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CAN-with-internal-IRC/m-p/603788#M4642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately you did not specify the device, so just generally.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are several requirements coming from the FlexCAN module, in summary…&lt;/P&gt;&lt;P&gt;- A valid CAN bit timing must be programmed, as indicated in RM.&lt;/P&gt;&lt;P&gt;- The peripheral clock frequency can not be smaller than the selected CPI clock frequency.&lt;/P&gt;&lt;P&gt;- There must be a minimum ratio between the peripheral clock frequency and the CAN bit rate, as specified in “Arbitration and Matching Timing” chapter of the RM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Nov 2016 09:18:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CAN-with-internal-IRC/m-p/603788#M4642</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2016-11-21T09:18:05Z</dc:date>
    </item>
  </channel>
</rss>