<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5604E Parallel Data Interface in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Parallel-Data-Interface/m-p/599108#M4418</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, this is OK. There's just one typo - there's missing VID_D4. So, you should use VID_D11 - VID_D4 on MPC5604E.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Oct 2016 07:12:11 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2016-10-04T07:12:11Z</dc:date>
    <item>
      <title>MPC5604E Parallel Data Interface</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Parallel-Data-Interface/m-p/599107#M4417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have connected 8 Video data lines from Digitizer [P0:7] to MPC5604E, MPC is having 12 Video data lines option VID_D[0:11], as I am using only 8 bit video, I am utilizing only 8 parallel video data lines. The issue is I have not connected P0 - VID_D0, P1-VID_D1, and so on till P7-VID_D7. The connection block diagram is attached please refer.&lt;/P&gt;&lt;P&gt;Will it work?&lt;span class="lia-inline-image-display-wrapper" image-alt="165341_165341.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/122309i40E26BB8FFC9B317/image-size/large?v=v2&amp;amp;px=999" role="button" title="165341_165341.png" alt="165341_165341.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1802i6C44FCB6C00CAC0D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Oct 2016 08:12:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Parallel-Data-Interface/m-p/599107#M4417</guid>
      <dc:creator>suhass</dc:creator>
      <dc:date>2016-10-01T08:12:49Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5604E Parallel Data Interface</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Parallel-Data-Interface/m-p/599108#M4418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, this is OK. There's just one typo - there's missing VID_D4. So, you should use VID_D11 - VID_D4 on MPC5604E.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Oct 2016 07:12:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Parallel-Data-Interface/m-p/599108#M4418</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2016-10-04T07:12:11Z</dc:date>
    </item>
  </channel>
</rss>