<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: Why doesn't eTPU Graphical Configuration Tool generated code compile?</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Why-doesn-t-eTPU-Graphical-Configuration-Tool-generated-code/m-p/597969#M4374</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mentioned macros are defined in ...\etpu\_utils\etpu_util.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is needed to include all files downloaded with using of eTPU function selector to your project as well as both files generated by GCT (for instance untitled_etpu_gct.c and untitled_etpu_gct.h).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also it is needed to call following following function from your user code&lt;BR /&gt;my_system_etpu_init();&lt;BR /&gt;my_system_etpu_start();&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and then you can use eTPU functions according its descriptive appnote&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 30 Sep 2016 14:26:10 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2016-09-30T14:26:10Z</dc:date>
    <item>
      <title>Why doesn't eTPU Graphical Configuration Tool generated code compile?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Why-doesn-t-eTPU-Graphical-Configuration-Tool-generated-code/m-p/597968#M4373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using eTPU GCT version 1.4.0.4. &amp;nbsp;I have read the application note about this&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2Fsoft_dev_tools%2Fdoc%2Fapp_note%2FAN4687.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4687.pdf&lt;/A&gt;&amp;nbsp;. &amp;nbsp;I downloaded the deliverable&amp;nbsp;from&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fwebapp%2Fetpu%2F" rel="nofollow" target="_blank"&gt;eTPU Funcion Selector|NXP&lt;/A&gt;&amp;nbsp;, such as FPM.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have taken the generated C module and included it in a CodeWarrior IDE version 5.9.0, Build 3510 project. &amp;nbsp;The macros defined in this file are not found any where in the eTPU Function set deliverable, or any of the generated code from the eTPU GCT. &amp;nbsp;FS_ETPU_VIS_OFF, for example, and many others. &amp;nbsp;Also, the structure pointer eTPU is missing.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I must be missing some header files. &amp;nbsp;What am I missing?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2016 23:18:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Why-doesn-t-eTPU-Graphical-Configuration-Tool-generated-code/m-p/597968#M4373</guid>
      <dc:creator>kentabacchi</dc:creator>
      <dc:date>2016-09-29T23:18:53Z</dc:date>
    </item>
    <item>
      <title>Re: Why doesn't eTPU Graphical Configuration Tool generated code compile?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Why-doesn-t-eTPU-Graphical-Configuration-Tool-generated-code/m-p/597969#M4374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mentioned macros are defined in ...\etpu\_utils\etpu_util.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is needed to include all files downloaded with using of eTPU function selector to your project as well as both files generated by GCT (for instance untitled_etpu_gct.c and untitled_etpu_gct.h).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also it is needed to call following following function from your user code&lt;BR /&gt;my_system_etpu_init();&lt;BR /&gt;my_system_etpu_start();&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and then you can use eTPU functions according its descriptive appnote&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Sep 2016 14:26:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Why-doesn-t-eTPU-Graphical-Configuration-Tool-generated-code/m-p/597969#M4374</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2016-09-30T14:26:10Z</dc:date>
    </item>
  </channel>
</rss>