<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: strange question about MPC5744p DMA in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/strange-question-about-MPC5744p-DMA/m-p/591642#M4292</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"You should mark the part of RAM, which is used for DMA transfers as non-cacheable."&lt;/P&gt;&lt;P&gt;------------- Is this configure SMPU_RGDn_WORD3.CI bit?&amp;nbsp; Thank you!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1690iE796D8CF2A6DB545/image-size/large?v=v2&amp;amp;px=999" title="捕获.PNG" alt="捕获.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Aug 2016 08:27:38 GMT</pubDate>
    <dc:creator>fyw</dc:creator>
    <dc:date>2016-08-11T08:27:38Z</dc:date>
    <item>
      <title>strange question about MPC5744p DMA</title>
      <link>https://community.nxp.com/t5/MPC5xxx/strange-question-about-MPC5744p-DMA/m-p/591639#M4289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i use dma transfer data from source --&amp;gt; destination,the program lists below.(&lt;SPAN&gt;&lt;STRONG&gt;See appendix for detailed code&lt;/STRONG&gt;&lt;/SPAN&gt;)&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;the question was caused by "&lt;SPAN style="color: #e23d39;"&gt;dly = destination[10];&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;" &lt;/P&gt;&lt;P&gt;if there is no read of destination[], for example&amp;nbsp; use "dly = 100" instead of " &lt;SPAN style="color: #e23d39;"&gt; dly = destination[10];&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;"&amp;nbsp;&amp;nbsp;&amp;nbsp; this program will &lt;SPAN style="color: #eb7a3d;"&gt;&lt;STRONG&gt;work well&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #eb7a3d;"&gt;&lt;SPAN style="color: #303030;"&gt;about dly = destination[X];&amp;nbsp; if X&amp;lt; 8&amp;nbsp; it seems that the first 8 data of&amp;nbsp;&amp;nbsp; destination[] cannot be update by dma&lt;/SPAN&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #303030;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if X&amp;gt;=8&amp;nbsp; it seems that the last 8 data of&amp;nbsp;&amp;nbsp; destination[] cannot be update by dma&amp;nbsp; (PS: i am not try every index)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;uint32_t source[16]={1,2,3,4,5,6,7,8,9,10,11,12,13,14,15,16};&amp;nbsp;&amp;nbsp; &lt;BR /&gt;uint32_t destination[16]={0,0,0,0, 0,0,0,0, 0,0,0,0, 0,0,0,0};&lt;/P&gt;&lt;P&gt;__attribute__ ((section(".text")))&lt;/P&gt;&lt;P&gt;int main(void)&lt;BR /&gt;{&lt;BR /&gt; uint32_t k,counter = 0;&lt;BR /&gt; uint32_t dly;&lt;BR /&gt; &lt;BR /&gt; xcptn_xmpl ();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Configure and Enable Interrupts */&lt;/P&gt;&lt;P&gt;CLK_Init();&lt;BR /&gt; AIPS_0_Init();&lt;BR /&gt; DMA_0_Init();&lt;/P&gt;&lt;P&gt;for(;;)&lt;BR /&gt; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN style="color: #e23d39;"&gt; dly = destination[10];&amp;nbsp;&amp;nbsp; /*this will cause strange phenomenon*/&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; for(k=0;k&amp;lt;dly;k++);&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //SoftTrig DMA&lt;BR /&gt;&amp;nbsp; DMA_0.TCD[0].CSR.B.START = 1u;&lt;BR /&gt;&amp;nbsp; while(DMA_0.TCD[0].CSR.B.DONE == 0u){};&lt;BR /&gt;&amp;nbsp; DMA_0.TCD[0].CSR.B.DONE = 0u;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; for(k=0;k&amp;lt;100000;k++);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*update the source data */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; for(k=0;k&amp;lt;16;k++)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; source[k] = counter;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; counter++;&lt;/P&gt;&lt;P&gt;}&lt;BR /&gt; &lt;BR /&gt; return 0;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338385"&gt;Example_Base.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 02:10:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/strange-question-about-MPC5744p-DMA/m-p/591639#M4289</guid>
      <dc:creator>fyw</dc:creator>
      <dc:date>2016-08-11T02:10:20Z</dc:date>
    </item>
    <item>
      <title>Re: strange question about MPC5744p DMA</title>
      <link>https://community.nxp.com/t5/MPC5xxx/strange-question-about-MPC5744p-DMA/m-p/591640#M4290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i find "&lt;EM&gt;&lt;STRONG&gt;disable dcache"&lt;/STRONG&gt; &lt;/EM&gt;before for(;;) can solve this problem&lt;/P&gt;&lt;P&gt;i wander why?&amp;nbsp; Is there any document about how to use cache?&amp;nbsp; Thank you very much!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void dcache_disable(void)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; register uint32_t val;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; E200CORE_SPR_GET(val,E200CORE_L1CSR0); /* L1CSR0 */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; val &amp;amp;= ~E200CORE_L1CSR0_CE;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; /* Memory Synchronize */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; E200CORE_SYNC();&lt;BR /&gt;&amp;nbsp;&amp;nbsp; /* Instruction Synchronize */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; E200CORE_ISYNC();&lt;BR /&gt;&amp;nbsp;&amp;nbsp; E200CORE_SPR_SET(E200CORE_L1CSR0,val);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; /* Instruction Synchronize */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; E200CORE_ISYNC();&lt;BR /&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 07:56:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/strange-question-about-MPC5744p-DMA/m-p/591640#M4290</guid>
      <dc:creator>fyw</dc:creator>
      <dc:date>2016-08-11T07:56:16Z</dc:date>
    </item>
    <item>
      <title>Re: strange question about MPC5744p DMA</title>
      <link>https://community.nxp.com/t5/MPC5xxx/strange-question-about-MPC5744p-DMA/m-p/591641#M4291</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;using cache together with DMA causes this issue. Explanation is fairly simple. When some lines of RAM are cached, debugger reads this lines via core and it finds the data at first in cache. When there is cache hit (line of RAM is present in cache), data are read from cache memory instead of RAM memory. But DMA writes data directly to the RAM. This causes &lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN&gt;inconsistencies&lt;/SPAN&gt;&lt;/SPAN&gt; between data in RAM and cache. There are different data in RAM and different data in cache.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You should mark the part of RAM, which is used for DMA transfers as non-cacheable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please look at the following document, which could be helpful for you:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="11363" data-containertype="14" data-objectid="330178" data-objecttype="102" href="https://community.nxp.com/docs/DOC-330178"&gt;e200 Core Training relevant to MPC55xx and MPC56xx device family&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 08:14:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/strange-question-about-MPC5744p-DMA/m-p/591641#M4291</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2016-08-11T08:14:17Z</dc:date>
    </item>
    <item>
      <title>Re: strange question about MPC5744p DMA</title>
      <link>https://community.nxp.com/t5/MPC5xxx/strange-question-about-MPC5744p-DMA/m-p/591642#M4292</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"You should mark the part of RAM, which is used for DMA transfers as non-cacheable."&lt;/P&gt;&lt;P&gt;------------- Is this configure SMPU_RGDn_WORD3.CI bit?&amp;nbsp; Thank you!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1690iE796D8CF2A6DB545/image-size/large?v=v2&amp;amp;px=999" title="捕获.PNG" alt="捕获.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 08:27:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/strange-question-about-MPC5744p-DMA/m-p/591642#M4292</guid>
      <dc:creator>fyw</dc:creator>
      <dc:date>2016-08-11T08:27:38Z</dc:date>
    </item>
    <item>
      <title>Re: strange question about MPC5744p DMA</title>
      <link>https://community.nxp.com/t5/MPC5xxx/strange-question-about-MPC5744p-DMA/m-p/591643#M4293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, this is the correct way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 08:31:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/strange-question-about-MPC5744p-DMA/m-p/591643#M4293</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2016-08-11T08:31:29Z</dc:date>
    </item>
    <item>
      <title>Re: strange question about MPC5744p DMA</title>
      <link>https://community.nxp.com/t5/MPC5xxx/strange-question-about-MPC5744p-DMA/m-p/591644#M4294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i read the smpu chapter and find that it mentioned the "&lt;STRONG&gt;master n&lt;/STRONG&gt;"&amp;nbsp; i wonder what is the "master n"?&amp;nbsp; thank you very much!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1699i199993051E326F9A/image-size/large?v=v2&amp;amp;px=999" title="捕获.PNG" alt="捕获.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;which(below) is the "master n"?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1793iE2AB447836ADBCD8/image-size/large?v=v2&amp;amp;px=999" title="1.PNG" alt="1.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 09:21:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/strange-question-about-MPC5744p-DMA/m-p/591644#M4294</guid>
      <dc:creator>fyw</dc:creator>
      <dc:date>2016-08-11T09:21:36Z</dc:date>
    </item>
    <item>
      <title>Re: strange question about MPC5744p DMA</title>
      <link>https://community.nxp.com/t5/MPC5xxx/strange-question-about-MPC5744p-DMA/m-p/591645#M4295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the n means the logical master ID. For example master 2 is DMA, master 3 is FlexRay and so on, see table 7-12&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 13:28:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/strange-question-about-MPC5744p-DMA/m-p/591645#M4295</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2016-08-11T13:28:51Z</dc:date>
    </item>
  </channel>
</rss>