<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: Nexus 3 frame format</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Nexus-3-frame-format/m-p/589057#M4236</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That's very helpful!.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since I am accessing the nexus interface through Lauterbach I have no access to the pins and I cannot see the separation between messages and packets but that's something I have to clarify somewhere else :-).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Jul 2016 13:32:13 GMT</pubDate>
    <dc:creator>manuelsaez</dc:creator>
    <dc:date>2016-07-20T13:32:13Z</dc:date>
    <item>
      <title>Nexus 3 frame format</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Nexus-3-frame-format/m-p/589055#M4234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;trying to decode the Nexus frames I came to a question that I could not find in the reference manual.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In chapter "63.7 Nexus message fields" the reference manual stays that:&lt;/P&gt;&lt;P&gt;"A packet may contain any number of fixed length fields, but may contain at most one variable length field."&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However in Charpter 63.3 TCODEs supported there are frame with up to 3 variable fields (like the Program Trace - Indirect Branch Messages). How can I know then what is the length of each field?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Manuel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2016 10:19:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Nexus-3-frame-format/m-p/589055#M4234</guid>
      <dc:creator>manuelsaez</dc:creator>
      <dc:date>2016-07-19T10:19:45Z</dc:date>
    </item>
    <item>
      <title>Re: Nexus 3 frame format</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Nexus-3-frame-format/m-p/589056#M4235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there are two different things: packet and message. Message can contain more packets.&lt;/P&gt;&lt;P&gt;Here is nice example for Indirect Branch Message:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38233i17B00305DB6F1C17/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Example:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38234i808170D366372C43/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;MSEO is used to indicate start/end of packet/message:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38245iD506ED5A99F647AF/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jul 2016 13:09:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Nexus-3-frame-format/m-p/589056#M4235</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2016-07-20T13:09:50Z</dc:date>
    </item>
    <item>
      <title>Re: Nexus 3 frame format</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Nexus-3-frame-format/m-p/589057#M4236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That's very helpful!.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since I am accessing the nexus interface through Lauterbach I have no access to the pins and I cannot see the separation between messages and packets but that's something I have to clarify somewhere else :-).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jul 2016 13:32:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Nexus-3-frame-format/m-p/589057#M4236</guid>
      <dc:creator>manuelsaez</dc:creator>
      <dc:date>2016-07-20T13:32:13Z</dc:date>
    </item>
  </channel>
</rss>