<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Run code from mpc5674Fflash, what need to be done? in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Run-code-from-mpc5674Fflash-what-need-to-be-done/m-p/581536#M4155</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;what IDE do you use? IDEs allow you to create project which already contains pre-defined startup files, linker files for RAM/flash target. For example, CodeWarrior IDE allows you to change the target anytime. Overlay is not necessary, of course.&lt;/P&gt;&lt;P&gt;Here you can find example with basic initialization:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-102744"&gt;Example XPC567XFKIT PinToggleStationery CW210&lt;/A&gt; &lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jun 2016 05:21:14 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2016-06-28T05:21:14Z</dc:date>
    <item>
      <title>Run code from mpc5674Fflash, what need to be done?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Run-code-from-mpc5674Fflash-what-need-to-be-done/m-p/581535#M4154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The mpc5674F has 4MB flash, so it can run from flash for a large&amp;nbsp; program&amp;nbsp; that is larger than 256K Ram. what do I need to do to make the program run smoothly.&amp;nbsp; linker file&amp;nbsp; need change ? do I need to ovelay the code memory map?&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jun 2016 22:55:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Run-code-from-mpc5674Fflash-what-need-to-be-done/m-p/581535#M4154</guid>
      <dc:creator>yanminhuang</dc:creator>
      <dc:date>2016-06-27T22:55:43Z</dc:date>
    </item>
    <item>
      <title>Re: Run code from mpc5674Fflash, what need to be done?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Run-code-from-mpc5674Fflash-what-need-to-be-done/m-p/581536#M4155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;what IDE do you use? IDEs allow you to create project which already contains pre-defined startup files, linker files for RAM/flash target. For example, CodeWarrior IDE allows you to change the target anytime. Overlay is not necessary, of course.&lt;/P&gt;&lt;P&gt;Here you can find example with basic initialization:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-102744"&gt;Example XPC567XFKIT PinToggleStationery CW210&lt;/A&gt; &lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jun 2016 05:21:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Run-code-from-mpc5674Fflash-what-need-to-be-done/m-p/581536#M4155</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2016-06-28T05:21:14Z</dc:date>
    </item>
  </channel>
</rss>