<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: MPC5777C CSE Boot MAC</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5777C-CSE-Boot-MAC/m-p/573834#M4113</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have spoken to application team and looks like we need to ask design directly.&lt;/P&gt;&lt;P&gt;I will inform you as soon as I will get reply from design.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Aug 2016 13:04:34 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2016-08-08T13:04:34Z</dc:date>
    <item>
      <title>MPC5777C CSE Boot MAC</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777C-CSE-Boot-MAC/m-p/573833#M4112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Quick question on the CSE - in the manual in the section for Secure Boot, it say that the MAC calculated over the secure boot region is compared with the stored BOOT_MAC, and if the stored value is zero, the new MAC is stored there instead.&amp;nbsp; If the secure boot section were to be modified at some point, is it possible to overwrite the value stored in BOOT_MAC?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Aug 2016 18:02:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777C-CSE-Boot-MAC/m-p/573833#M4112</guid>
      <dc:creator>jeffcampbell</dc:creator>
      <dc:date>2016-08-04T18:02:31Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777C CSE Boot MAC</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777C-CSE-Boot-MAC/m-p/573834#M4113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have spoken to application team and looks like we need to ask design directly.&lt;/P&gt;&lt;P&gt;I will inform you as soon as I will get reply from design.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Aug 2016 13:04:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777C-CSE-Boot-MAC/m-p/573834#M4113</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2016-08-08T13:04:34Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777C CSE Boot MAC</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777C-CSE-Boot-MAC/m-p/573835#M4114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt; Yes, it is possible to change the BOOT_MAC if secure boot section needs to be modified. But this assumes some conditions and there can be different scenarios. Please refer to the CSE App Note "AN4234-Using CSE" for detailed description. Particularly refer the "Section 2.10: Code flash update procedure" which discusses this question. There are also SW examples for this App Note. Please see example "D.1.2: Reprogramming of a programmed part".&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 04:26:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777C-CSE-Boot-MAC/m-p/573835#M4114</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2016-08-10T04:26:57Z</dc:date>
    </item>
  </channel>
</rss>