<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KIT33908MBEVBE CAN in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/KIT33908MBEVBE-CAN/m-p/557086#M3941</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the Debug mode is activated (debug jumper set) the CAN transceiver is set to Normal operation mode and you are able to communicate normally.&lt;/P&gt;&lt;P&gt;Without this jumper the CAN transceiver is kept in Sleep mode by default. In that case, the CANH and CANL pins are pulled down to GND via the internal R&lt;SUB&gt;IN&lt;/SUB&gt; resistor, the TXD and RXD pins are pulled down to GND, both driver and receiver are OFF.&lt;/P&gt;&lt;P&gt;You need to write to the CAN_LIN MODE Register and set CAN_mode_1:0 bits to configure Normal operational mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Aug 2016 08:46:27 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2016-08-02T08:46:27Z</dc:date>
    <item>
      <title>KIT33908MBEVBE CAN</title>
      <link>https://community.nxp.com/t5/MPC5xxx/KIT33908MBEVBE-CAN/m-p/557085#M3940</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using the KIT and I can configure the SBC and answer correctly to the WD&lt;/P&gt;&lt;P&gt;I noticed that the behavior of CAN is different with or without the debug jumper&lt;/P&gt;&lt;P&gt;The power of CAN CAN_5V is high in both mode&lt;/P&gt;&lt;P&gt;Without debug jumper the pin CANH and CANL are inactive and with level 0V while in the pin CAN_TX there is signals&lt;/P&gt;&lt;P&gt;With debug jumper the signal arrives correctly also to CANH and CANL&lt;/P&gt;&lt;P&gt;There is some other particular configuration on EVB or on SBC to apply?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Manuela&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Aug 2016 10:41:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/KIT33908MBEVBE-CAN/m-p/557085#M3940</guid>
      <dc:creator>manuelaielo</dc:creator>
      <dc:date>2016-08-01T10:41:07Z</dc:date>
    </item>
    <item>
      <title>Re: KIT33908MBEVBE CAN</title>
      <link>https://community.nxp.com/t5/MPC5xxx/KIT33908MBEVBE-CAN/m-p/557086#M3941</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the Debug mode is activated (debug jumper set) the CAN transceiver is set to Normal operation mode and you are able to communicate normally.&lt;/P&gt;&lt;P&gt;Without this jumper the CAN transceiver is kept in Sleep mode by default. In that case, the CANH and CANL pins are pulled down to GND via the internal R&lt;SUB&gt;IN&lt;/SUB&gt; resistor, the TXD and RXD pins are pulled down to GND, both driver and receiver are OFF.&lt;/P&gt;&lt;P&gt;You need to write to the CAN_LIN MODE Register and set CAN_mode_1:0 bits to configure Normal operational mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Aug 2016 08:46:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/KIT33908MBEVBE-CAN/m-p/557086#M3941</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2016-08-02T08:46:27Z</dc:date>
    </item>
    <item>
      <title>Re: KIT33908MBEVBE CAN</title>
      <link>https://community.nxp.com/t5/MPC5xxx/KIT33908MBEVBE-CAN/m-p/557087#M3942</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Petr&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;When the Debug mode is activated (debug jumper set) the CAN transceiver is set to Normal operation mode. Under the circumstances,do I need to initialize the SBC chip to enable transceiver by codes?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thanks &amp;nbsp;a lot.&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE data-fulltext="" data-placeholder="翻译" dir="ltr"&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Dec 2016 07:32:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/KIT33908MBEVBE-CAN/m-p/557087#M3942</guid>
      <dc:creator>lmonologue</dc:creator>
      <dc:date>2016-12-21T07:32:44Z</dc:date>
    </item>
  </channel>
</rss>