<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: XXXX Bus Error - No Opcode</title>
    <link>https://community.nxp.com/t5/MPC5xxx/XXXX-Bus-Error-No-Opcode/m-p/556512#M3922</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;this might be caused by debugger memory window being opened pointing to illegal/uninitialized memory when the debugger is starting. Also if variables are displayed in Variable window. If this is the case I'd suggest you to close the memory window (or set the address to 0), remove variables from Variable Window&amp;nbsp; and reset the MCU or download the code again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Aug 2016 09:05:17 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2016-08-02T09:05:17Z</dc:date>
    <item>
      <title>XXXX Bus Error - No Opcode</title>
      <link>https://community.nxp.com/t5/MPC5xxx/XXXX-Bus-Error-No-Opcode/m-p/556511#M3921</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I debug TRK-MPC5604B with codewarrior 2.10, I see below issue:&lt;/P&gt;&lt;P&gt;_start XXXX Bus Error - No Opcode&lt;/P&gt;&lt;P&gt;Error: Error in Once status register during instruction execution.&lt;/P&gt;&lt;P&gt;use 'gotil main' command to run until main procedure&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Aug 2016 11:20:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/XXXX-Bus-Error-No-Opcode/m-p/556511#M3921</guid>
      <dc:creator>langwu</dc:creator>
      <dc:date>2016-08-01T11:20:51Z</dc:date>
    </item>
    <item>
      <title>Re: XXXX Bus Error - No Opcode</title>
      <link>https://community.nxp.com/t5/MPC5xxx/XXXX-Bus-Error-No-Opcode/m-p/556512#M3922</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;this might be caused by debugger memory window being opened pointing to illegal/uninitialized memory when the debugger is starting. Also if variables are displayed in Variable window. If this is the case I'd suggest you to close the memory window (or set the address to 0), remove variables from Variable Window&amp;nbsp; and reset the MCU or download the code again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Aug 2016 09:05:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/XXXX-Bus-Error-No-Opcode/m-p/556512#M3922</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2016-08-02T09:05:17Z</dc:date>
    </item>
  </channel>
</rss>