<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: STM Timer running  in STNDBY mode in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/STM-Timer-running-in-STNDBY-mode/m-p/537297#M3633</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have shared simple test code using STM here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-332233"&gt;Example MPC5748G Standby mode GHS614&lt;/A&gt; &lt;/P&gt;&lt;P&gt;1. Yes.&lt;/P&gt;&lt;P&gt;2. In standby, it is necessary to use FXOSC because system clock is not available.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36953i58C1B2A8F59FF720/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;3. STM_0 is active in standby.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36996i3CFC5997963A6313/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Jul 2016 14:10:27 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2016-07-25T14:10:27Z</dc:date>
    <item>
      <title>STM Timer running  in STNDBY mode</title>
      <link>https://community.nxp.com/t5/MPC5xxx/STM-Timer-running-in-STNDBY-mode/m-p/537296#M3632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We wanted to start a STM timer just before entering into STBY mode in MPC5748G. This is to implement a periodic check in the SLEEP mode. Could you please answer following queries about this .&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. During the timeout , to service the STM interupt whether power mode will be changed automatically to DRUN on a timer interrupt?&lt;/P&gt;&lt;P&gt;2. STM timer is clocked by 80MHZ in run mode, what will be the clock frequency and clock source in STBY mode, is it configurable?&lt;/P&gt;&lt;P&gt;3. In case STM is not active in STBY which other timer can be used for period interrupt.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jul 2016 13:19:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/STM-Timer-running-in-STNDBY-mode/m-p/537296#M3632</guid>
      <dc:creator>kpitsupportshas</dc:creator>
      <dc:date>2016-07-25T13:19:05Z</dc:date>
    </item>
    <item>
      <title>Re: STM Timer running  in STNDBY mode</title>
      <link>https://community.nxp.com/t5/MPC5xxx/STM-Timer-running-in-STNDBY-mode/m-p/537297#M3633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have shared simple test code using STM here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-332233"&gt;Example MPC5748G Standby mode GHS614&lt;/A&gt; &lt;/P&gt;&lt;P&gt;1. Yes.&lt;/P&gt;&lt;P&gt;2. In standby, it is necessary to use FXOSC because system clock is not available.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36953i58C1B2A8F59FF720/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;3. STM_0 is active in standby.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36996i3CFC5997963A6313/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jul 2016 14:10:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/STM-Timer-running-in-STNDBY-mode/m-p/537297#M3633</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2016-07-25T14:10:27Z</dc:date>
    </item>
  </channel>
</rss>