<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: MPC5553MZP132 Power down sequence</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5553MZP132-Power-down-sequence/m-p/531985#M3579</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;VRC33 is recommended to have connected to 3.3V to remove power sequence requirements. But if you have it connected to ground, then sections 3.7.2 and 3.7.3 take place.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could I see your power down sequence?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think following sentence answers your question:&lt;/P&gt;&lt;P&gt;"VDDSYN or the RESET power must decrease to less than 2.0 V before the VDD power increases to its operating range."&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Jul 2016 10:50:51 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2016-07-26T10:50:51Z</dc:date>
    <item>
      <title>MPC5553MZP132 Power down sequence</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5553MZP132-Power-down-sequence/m-p/531984#M3578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am looking at the power down sequence paragraph 3.7.3 of the MPC5553 data sheet and I would like to request clarification, to understand the power down sequence requirement.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In our application VRC33 is hardwired to GND.&lt;/P&gt;&lt;P&gt;VDD =1.5V and VDDSYN =3.3V&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I remove 5 VDC which generates the 3.3V and the 1.5V I get an output glitch on 10 different pins which are expected to stay low during power down.&lt;/P&gt;&lt;P&gt;These pins are ADDR13, ADDR12, ADDR11, ADDR10, ADDR9, ADDR8, CS3, CS2, CS1 AND CS0.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When the unexpected low to high glitch occurs on these outputs the voltages are as follows:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;VDD = 1.5V&lt;/P&gt;&lt;P&gt;VDDSYN =2.2V&lt;/P&gt;&lt;P&gt;5V = 3.3V&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Should my VDDSYN be below 2.0V when we produce a RESET?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jul 2016 12:25:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5553MZP132-Power-down-sequence/m-p/531984#M3578</guid>
      <dc:creator>Carl725</dc:creator>
      <dc:date>2016-07-22T12:25:28Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5553MZP132 Power down sequence</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5553MZP132-Power-down-sequence/m-p/531985#M3579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;VRC33 is recommended to have connected to 3.3V to remove power sequence requirements. But if you have it connected to ground, then sections 3.7.2 and 3.7.3 take place.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could I see your power down sequence?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think following sentence answers your question:&lt;/P&gt;&lt;P&gt;"VDDSYN or the RESET power must decrease to less than 2.0 V before the VDD power increases to its operating range."&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jul 2016 10:50:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5553MZP132-Power-down-sequence/m-p/531985#M3579</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2016-07-26T10:50:51Z</dc:date>
    </item>
  </channel>
</rss>