<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: wait instruction in MPC5633M in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/wait-instruction-in-MPC5633M/m-p/303419#M354</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The “wait 1,0” instruction (op code 0x7C20007C) is not implemented on the MPC563xM and the execution leads to the IVOR6 (illegal/unimplemented instruction exception).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So that sentence in the EREF RM is not valid for the MPC563xM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Mar 2014 10:14:14 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2014-03-27T10:14:14Z</dc:date>
    <item>
      <title>wait instruction in MPC5633M</title>
      <link>https://community.nxp.com/t5/MPC5xxx/wait-instruction-in-MPC5633M/m-p/303418#M353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need to use 'wait' instruction with WC field equal 1. Opcode of the instruction according to &lt;/P&gt;&lt;P&gt;EREF 2.0: A Programmer’s Reference Manual for Freescale Power Architecture® Processors&lt;/P&gt;&lt;P&gt;and Power ISA™ Version 2.07&lt;/P&gt;&lt;P&gt;shall be:&amp;nbsp; 0x7C20007C&lt;/P&gt;&lt;P&gt;But I'm getting program exception. Only when I use 0x7C00007C (wait with WC=0), no exception is generated.&lt;/P&gt;&lt;P&gt;Documents above read that if some WC other than 0 is not implemented, bahaviour of the instruction should equal to the one with WC = 0.&lt;/P&gt;&lt;P&gt;I'd like to ask if the instruction (wait with WC=1)&amp;nbsp; is really not implemented or if I do something wrong.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;&lt;P&gt;Pavel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Mar 2014 12:58:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/wait-instruction-in-MPC5633M/m-p/303418#M353</guid>
      <dc:creator>pavelhavlik</dc:creator>
      <dc:date>2014-03-25T12:58:24Z</dc:date>
    </item>
    <item>
      <title>Re: wait instruction in MPC5633M</title>
      <link>https://community.nxp.com/t5/MPC5xxx/wait-instruction-in-MPC5633M/m-p/303419#M354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The “wait 1,0” instruction (op code 0x7C20007C) is not implemented on the MPC563xM and the execution leads to the IVOR6 (illegal/unimplemented instruction exception).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So that sentence in the EREF RM is not valid for the MPC563xM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Mar 2014 10:14:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/wait-instruction-in-MPC5633M/m-p/303419#M354</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2014-03-27T10:14:14Z</dc:date>
    </item>
    <item>
      <title>Re: wait instruction in MPC5633M</title>
      <link>https://community.nxp.com/t5/MPC5xxx/wait-instruction-in-MPC5633M/m-p/303420#M355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Petr,&lt;/P&gt;&lt;P&gt;thank you for the clarification.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pavel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Mar 2014 16:13:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/wait-instruction-in-MPC5633M/m-p/303420#M355</guid>
      <dc:creator>pavelhavlik</dc:creator>
      <dc:date>2014-03-27T16:13:48Z</dc:date>
    </item>
  </channel>
</rss>