<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Shadow Flash direct programming in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Shadow-Flash-direct-programming/m-p/529410#M3539</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Quick question - I'm attempting to alter shadow flash (fully aware of the risks; I've successfully done it already and am experimenting with the process).&amp;nbsp; Is it possible to edit the shadow block directly during the process of programming the chip (i.e. have a defined data section that gets loaded directly to Shadow Block A alongside the rest of the main program), or can it only be modified by a function executing from RAM?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Jul 2016 20:41:50 GMT</pubDate>
    <dc:creator>jeffcampbell</dc:creator>
    <dc:date>2016-07-21T20:41:50Z</dc:date>
    <item>
      <title>Shadow Flash direct programming</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Shadow-Flash-direct-programming/m-p/529410#M3539</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Quick question - I'm attempting to alter shadow flash (fully aware of the risks; I've successfully done it already and am experimenting with the process).&amp;nbsp; Is it possible to edit the shadow block directly during the process of programming the chip (i.e. have a defined data section that gets loaded directly to Shadow Block A alongside the rest of the main program), or can it only be modified by a function executing from RAM?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jul 2016 20:41:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Shadow-Flash-direct-programming/m-p/529410#M3539</guid>
      <dc:creator>jeffcampbell</dc:creator>
      <dc:date>2016-07-21T20:41:50Z</dc:date>
    </item>
    <item>
      <title>Re: Shadow Flash direct programming</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Shadow-Flash-direct-programming/m-p/529411#M3540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it is possible, if particular programmer have defined programming algorithm for shadow flash (for instance PeMicro debugger have them prepared …\pemicro\algorithms\shadow\).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Production programmers should be capable to do it as well as it can be just a requirement to set up censorship during production programming.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jul 2016 07:05:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Shadow-Flash-direct-programming/m-p/529411#M3540</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2016-07-22T07:05:02Z</dc:date>
    </item>
  </channel>
</rss>