<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPC5604 CMP output pad in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5604-CMP-output-pad/m-p/521220#M3516</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir or Mandam,&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a problem when configuring CMP module. I use the CMP2_IN[1] as the positive input of CMP, 3.3V as the negative input of CMP, ccording to the datasheet, the CMP2_O (PB10) should change with the result of the comparasion, however, in fact the CMP2_O (PB10) is always high whatever the result of the comparasion is.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Attached is my project, could you please to tell me what's wrong with my program?&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338322"&gt;mpc5748g_Z4_1.rar&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 08:27:02 GMT</pubDate>
    <dc:creator>shifeiqian</dc:creator>
    <dc:date>2016-06-15T08:27:02Z</dc:date>
    <item>
      <title>MPC5604 CMP output pad</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5604-CMP-output-pad/m-p/521220#M3516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir or Mandam,&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a problem when configuring CMP module. I use the CMP2_IN[1] as the positive input of CMP, 3.3V as the negative input of CMP, ccording to the datasheet, the CMP2_O (PB10) should change with the result of the comparasion, however, in fact the CMP2_O (PB10) is always high whatever the result of the comparasion is.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Attached is my project, could you please to tell me what's wrong with my program?&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338322"&gt;mpc5748g_Z4_1.rar&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 08:27:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5604-CMP-output-pad/m-p/521220#M3516</guid>
      <dc:creator>shifeiqian</dc:creator>
      <dc:date>2016-06-15T08:27:02Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5604 CMP output pad</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5604-CMP-output-pad/m-p/521221#M3517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Without any deeper study of your complex code I see you don’t have set SIUL_MSCR26[SSS] to 0x3 what selects CMP2_O functionality.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 11:03:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5604-CMP-output-pad/m-p/521221#M3517</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2016-06-16T11:03:47Z</dc:date>
    </item>
  </channel>
</rss>