<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5775K multicore in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515373#M3378</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when you open Multilink Universal, there is jumper JP10, which could unconnected, connected to 3.3V or connected to 5V. This power supply could be used for EVB power supply and sometimes it could be a source of the problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Jun 2016 12:29:42 GMT</pubDate>
    <dc:creator>martin_kovar</dc:creator>
    <dc:date>2016-06-07T12:29:42Z</dc:date>
    <item>
      <title>MPC5775K multicore</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515363#M3368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm working with MPC5775K now. And I want it to work in the multicore mode. But it seems that only one core is working in the right way. I set breakpoints in other two cores. There is no action.&amp;nbsp; I call the function 'hw_init()' in the main core. But is doesn't work. Any suggestions?&lt;/P&gt;&lt;P&gt;Thanks. &lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ron&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="153012_153012.bmp"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/121727i0B404E7872F2D333/image-size/large?v=v2&amp;amp;px=999" role="button" title="153012_153012.bmp" alt="153012_153012.bmp" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="xx.bmp"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59662i1F2829135CA70F26/image-size/large?v=v2&amp;amp;px=999" role="button" title="xx.bmp" alt="xx.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jun 2016 13:29:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515363#M3368</guid>
      <dc:creator>ronliu</dc:creator>
      <dc:date>2016-06-06T13:29:45Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775K multicore</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515364#M3369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I created some breakpoints among these three cores in the project. But only one core could react. Other two cores seemed not able to work.&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/PetrS"&gt;PetrS&lt;/A&gt;​@&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 02:57:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515364#M3369</guid>
      <dc:creator>ronliu</dc:creator>
      <dc:date>2016-06-07T02:57:19Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775K multicore</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515365#M3370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at this example &lt;A href="https://community.nxp.com/docs/DOC-329809"&gt;Example MPC5775K PinToggleStationery S32DS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tested it and it works correct. I call function boot_cores to run both z7 cores instead of hw_init function. But do not forget look to the startup.s file. In default project, hw_init function is called before you jump to the main function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the screen of z4 core. You can see that both z7 cores started to run&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60722i451B3AD8BEF220A7/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you click on the marked line, you can watch z7a source code&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60726iB7A882C7673976FE/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and also z7b source code&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_4.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60738iDC2D7E94CF87A074/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: S32DS has a problem with "one line" while loop. If you have for example this code:&lt;/P&gt;&lt;P&gt;while(1)&lt;/P&gt;&lt;P&gt;{counter++;}&lt;/P&gt;&lt;P&gt;and you click on &lt;STRONG&gt;step over&lt;/STRONG&gt; or &lt;STRONG&gt;step into&lt;/STRONG&gt;, debugger stop working and it may seen the core is not running correct.&lt;/P&gt;&lt;P&gt;I hope this issue will be fixed in the next release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 07:20:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515365#M3370</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2016-06-07T07:20:34Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775K multicore</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515366#M3371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin,&lt;/P&gt;&lt;P&gt;Thanks. But I come across the same problem when I try to download the project.&lt;/P&gt;&lt;P&gt;It really confused me now&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ron&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="58.bmp"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60752i2CA16A3AB85A6F48/image-size/large?v=v2&amp;amp;px=999" role="button" title="58.bmp" alt="58.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 08:44:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515366#M3371</guid>
      <dc:creator>ronliu</dc:creator>
      <dc:date>2016-06-07T08:44:43Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775K multicore</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515367#M3372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="11.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38980i54F65EEF60771C89/image-size/large?v=v2&amp;amp;px=999" role="button" title="11.png" alt="11.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;There are all the processes running in my computer.&amp;nbsp; So I couldn't find those about PPC. I'm not clear what was wrong.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 09:17:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515367#M3372</guid>
      <dc:creator>ronliu</dc:creator>
      <dc:date>2016-06-07T09:17:08Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775K multicore</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515368#M3373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what password do you enter, while the debug session starting?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60793iDFF922F4B965342A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This is default password, which must not be used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Instead of this password, please use DEAD_DEED_FADE_BADE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you use correct password, please try to update PeMicro debugger firmware. Download the drivers from following link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/downloads/download_file.cfm?download_id=346" title="http://www.pemicro.com/downloads/download_file.cfm?download_id=346"&gt;http://www.pemicro.com/downloads/download_file.cfm?download_id=346&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which MPC5775K mask you use? I have 0N76P and I am not able to reproduce the problem. Which operating system you use?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 10:14:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515368#M3373</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2016-06-07T10:14:24Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775K multicore</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515369#M3374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Martin,&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;P&gt;I tried to update the firmware.&amp;nbsp; But the problem still existed.&amp;nbsp; &lt;/P&gt;&lt;P&gt;And I am using 0N38M. The OS is windows 10.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="7.bmp"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60800i1E2455B98DEF2A33/image-size/large?v=v2&amp;amp;px=999" role="button" title="7.bmp" alt="7.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 10:58:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515369#M3374</guid>
      <dc:creator>ronliu</dc:creator>
      <dc:date>2016-06-07T10:58:41Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775K multicore</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515370#M3375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you have connected JP10 jumper in the debugger, try to disconnect.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you installed this drivers to you OS?&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/downloads/download_file.cfm?download_id=53" title="http://www.pemicro.com/downloads/download_file.cfm?download_id=53"&gt;http://www.pemicro.com/downloads/download_file.cfm?download_id=53&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do not have WIN10 available right now to check it, but I will try to do it as soon as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 11:29:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515370#M3375</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2016-06-07T11:29:00Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775K multicore</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515371#M3376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually. When I debug other projects, it works well. But I try to download your project. It isn't able to work. It is really strange. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 12:08:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515371#M3376</guid>
      <dc:creator>ronliu</dc:creator>
      <dc:date>2016-06-07T12:08:32Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775K multicore</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515372#M3377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what do you mean about JP10 jumper?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 12:22:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515372#M3377</guid>
      <dc:creator>ronliu</dc:creator>
      <dc:date>2016-06-07T12:22:56Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775K multicore</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515373#M3378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when you open Multilink Universal, there is jumper JP10, which could unconnected, connected to 3.3V or connected to 5V. This power supply could be used for EVB power supply and sometimes it could be a source of the problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 12:29:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515373#M3378</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2016-06-07T12:29:42Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775K multicore</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515374#M3379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin,&lt;/P&gt;&lt;P&gt;I found a strange thing that the route of the file is C:\Users\b55689... But I created my project in D disk. How do I change the configuration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="29.bmp"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60837i12B816464AFC23FF/image-size/large?v=v2&amp;amp;px=999" role="button" title="29.bmp" alt="29.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 13:09:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515374#M3379</guid>
      <dc:creator>ronliu</dc:creator>
      <dc:date>2016-06-07T13:09:59Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775K multicore</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515375#M3380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please download my project and import it to your workspace.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Choose Existing Projects and click next:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60840iF723601317BB42AE/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Select directory, where the downloaded project is placed and check all project folders (sorry for figure, I have already this project in my workspace) and click finish. You can also copy the project to workspace folder.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60844i603B8AC993CE78C2/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 13:15:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515375#M3380</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2016-06-07T13:15:40Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775K multicore</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515376#M3381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Martin,&lt;/P&gt;&lt;P&gt;I changed the configuration of the project. The IDE didn't report the errors. But after I download the project. There only one elf in the debug window. So other two cores couldn't work correctly. Is there something wrong with my configuration?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="QQ截图20160607214655.bmp"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60848i39FDEDBFEE980CB2/image-size/large?v=v2&amp;amp;px=999" role="button" title="QQ截图20160607214655.bmp" alt="QQ截图20160607214655.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 13:53:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515376#M3381</guid>
      <dc:creator>ronliu</dc:creator>
      <dc:date>2016-06-07T13:53:23Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775K multicore</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515377#M3382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin,&lt;/P&gt;&lt;P&gt;My project works correctly now. I&amp;nbsp; must call function boot_cores() to run both z7 cores instead of&amp;nbsp; default hw_init() function. And I call the boot_cores() after jumping to the main(). &lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ron&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jun 2016 02:35:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-multicore/m-p/515377#M3382</guid>
      <dc:creator>ronliu</dc:creator>
      <dc:date>2016-06-08T02:35:40Z</dc:date>
    </item>
  </channel>
</rss>