<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic [MPC5645S] Display 16bpp image using external flash memory in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5645S-Display-16bpp-image-using-external-flash-memory/m-p/512380#M3311</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm Working with MPC5645S and code warrior IDE 5.9.&lt;/P&gt;&lt;P&gt;Following the document "AN4865". I have the DCU3 configured and running with a TFT of 800x480 using a Nominal clock of 32MHz.&lt;/P&gt;&lt;P&gt;We display correctly small images (size: 16x6 pixels) from the External memory. &lt;/P&gt;&lt;P&gt;Unfortunately when we use a image that have for example 300x300 pixels, this image was not read correctly.&lt;/P&gt;&lt;P&gt;To read these images I use the "AHB address" to set the beginning address of layer data. (DCU.LAYER[6].CTRLDESCL3.R = 0x70000000)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please, could somebody help me with this problem?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Josep Gorgues&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Mar 2016 10:21:36 GMT</pubDate>
    <dc:creator>josepgorgues</dc:creator>
    <dc:date>2016-03-30T10:21:36Z</dc:date>
    <item>
      <title>[MPC5645S] Display 16bpp image using external flash memory</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5645S-Display-16bpp-image-using-external-flash-memory/m-p/512380#M3311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm Working with MPC5645S and code warrior IDE 5.9.&lt;/P&gt;&lt;P&gt;Following the document "AN4865". I have the DCU3 configured and running with a TFT of 800x480 using a Nominal clock of 32MHz.&lt;/P&gt;&lt;P&gt;We display correctly small images (size: 16x6 pixels) from the External memory. &lt;/P&gt;&lt;P&gt;Unfortunately when we use a image that have for example 300x300 pixels, this image was not read correctly.&lt;/P&gt;&lt;P&gt;To read these images I use the "AHB address" to set the beginning address of layer data. (DCU.LAYER[6].CTRLDESCL3.R = 0x70000000)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please, could somebody help me with this problem?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Josep Gorgues&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Mar 2016 10:21:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5645S-Display-16bpp-image-using-external-flash-memory/m-p/512380#M3311</guid>
      <dc:creator>josepgorgues</dc:creator>
      <dc:date>2016-03-30T10:21:36Z</dc:date>
    </item>
  </channel>
</rss>