<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Running code without the USB multilink interface on MPC5668EVB</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Running-code-without-the-USB-multilink-interface-on-MPC5668EVB/m-p/293667#M294</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working on an application for the MPC5668G µC. The application is compiled with codeWarrior and Flashed to memory through the USB multilink interface. I am able to run the application with Code Warrior ICD PPC nexus, but unfortunately when I start the board withouth the multilink interface connected, the application does not run. Is there a special location to Flash the application to be able tu run without the ICD?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Sep 2013 14:28:52 GMT</pubDate>
    <dc:creator>pierreschmidt</dc:creator>
    <dc:date>2013-09-09T14:28:52Z</dc:date>
    <item>
      <title>Running code without the USB multilink interface on MPC5668EVB</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Running-code-without-the-USB-multilink-interface-on-MPC5668EVB/m-p/293667#M294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working on an application for the MPC5668G µC. The application is compiled with codeWarrior and Flashed to memory through the USB multilink interface. I am able to run the application with Code Warrior ICD PPC nexus, but unfortunately when I start the board withouth the multilink interface connected, the application does not run. Is there a special location to Flash the application to be able tu run without the ICD?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Sep 2013 14:28:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Running-code-without-the-USB-multilink-interface-on-MPC5668EVB/m-p/293667#M294</guid>
      <dc:creator>pierreschmidt</dc:creator>
      <dc:date>2013-09-09T14:28:52Z</dc:date>
    </item>
    <item>
      <title>Re: Running code without the USB multilink interface on MPC5668EVB</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Running-code-without-the-USB-multilink-interface-on-MPC5668EVB/m-p/293668#M295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There may be an issue with the SRAM init and/or MMU init upon startup.&lt;/P&gt;&lt;P&gt;Attached you can find an “MPC5668G-PinToggleStationery” project, which work well as standalone application too.&lt;/P&gt;&lt;P&gt;You may use it as a base project for your development.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Sep 2013 12:56:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Running-code-without-the-USB-multilink-interface-on-MPC5668EVB/m-p/293668#M295</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2013-09-25T12:56:22Z</dc:date>
    </item>
    <item>
      <title>Re: Running code without the USB multilink interface on MPC5668EVB</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Running-code-without-the-USB-multilink-interface-on-MPC5668EVB/m-p/293669#M296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've seen your answer only today. I will try your attachement and let you know if it helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Oct 2013 20:22:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Running-code-without-the-USB-multilink-interface-on-MPC5668EVB/m-p/293669#M296</guid>
      <dc:creator>pierreschmidt</dc:creator>
      <dc:date>2013-10-10T20:22:27Z</dc:date>
    </item>
  </channel>
</rss>