<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: MPC5775B – Application to RAppID Bootloader transition</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5775B-Application-to-RAppID-Bootloader-transition/m-p/2415878#M28628</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37795"&gt;@lukaszadrapa&lt;/a&gt;&amp;nbsp;Can you help me out on this topic?&lt;/P&gt;</description>
    <pubDate>Thu, 24 Sep 2026 04:41:23 GMT</pubDate>
    <dc:creator>NXP_007</dc:creator>
    <dc:date>2026-09-24T04:41:23Z</dc:date>
    <item>
      <title>MPC5775B – Application to RAppID Bootloader transition</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775B-Application-to-RAppID-Bootloader-transition/m-p/2412743#M28607</link>
      <description>&lt;P&gt;Hello NXP Team, I am using &lt;STRONG&gt;MPC5775B with RAppID Bootloader&lt;/STRONG&gt; for CAN flashing.&lt;BR /&gt;I do not have the RAppID FBL source code, so I cannot modify the existing FBL.&lt;BR /&gt;Is there a &lt;STRONG&gt;supported mechanism for the running application to request the existing RAppID FBL to enter programming mode&lt;/STRONG&gt;?&lt;BR /&gt;If yes, what is the required Application → FBL entry sequence for MPC5775B?&lt;BR /&gt;Does this require a specific reset/boot mechanism, or does RAppID provide another way to request FBL from the application?&lt;/P&gt;</description>
      <pubDate>Thu, 10 Sep 2026 12:39:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775B-Application-to-RAppID-Bootloader-transition/m-p/2412743#M28607</guid>
      <dc:creator>NXP_007</dc:creator>
      <dc:date>2026-09-10T12:39:23Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775B – Application to RAppID Bootloader transition</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775B-Application-to-RAppID-Bootloader-transition/m-p/2412931#M28609</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;There is no built-in, documented API in the RAppID FBL for the running application to programmatically request FBL entry. The RAppID bootloader for MPC57xx is a closed-binary, flash-resident bootloader (distributed as a pre-compiled .rbf file) with no source code provided and no modification possible. &lt;BR /&gt;The standard mechanism to trigger it is a reset + boot-time flag check, not a runtime call from the application.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Fri, 11 Sep 2026 07:14:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775B-Application-to-RAppID-Bootloader-transition/m-p/2412931#M28609</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2026-09-11T07:14:38Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775B – Application to RAppID Bootloader transition</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775B-Application-to-RAppID-Bootloader-transition/m-p/2413556#M28613</link>
      <description>Thanks Peter. Understood that the mechanism is a reset followed by a boot-time flag check. Since we do not have the RAppID FBL source code, could you please clarify what boot-time flag/condition the RAppID FBL for MPC5775B checks, and how the application can set/request it before reset?&lt;BR /&gt;&lt;BR /&gt;Is this a specific RAM address/magic value, reset-cause condition, configuration field, or another mechanism? If there is an application-side procedure or documentation for setting this flag, could you please share it?</description>
      <pubDate>Tue, 15 Sep 2026 05:59:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775B-Application-to-RAppID-Bootloader-transition/m-p/2413556#M28613</guid>
      <dc:creator>NXP_007</dc:creator>
      <dc:date>2026-09-15T05:59:38Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775B – Application to RAppID Bootloader transition</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775B-Application-to-RAppID-Bootloader-transition/m-p/2414847#M28622</link>
      <description>&lt;P&gt;Please do let me know if you have any solution to the problem.&lt;BR /&gt;&lt;BR /&gt;Thank you,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Sep 2026 06:02:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775B-Application-to-RAppID-Bootloader-transition/m-p/2414847#M28622</guid>
      <dc:creator>NXP_007</dc:creator>
      <dc:date>2026-09-21T06:02:02Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775B – Application to RAppID Bootloader transition</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775B-Application-to-RAppID-Bootloader-transition/m-p/2415878#M28628</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37795"&gt;@lukaszadrapa&lt;/a&gt;&amp;nbsp;Can you help me out on this topic?&lt;/P&gt;</description>
      <pubDate>Thu, 24 Sep 2026 04:41:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775B-Application-to-RAppID-Bootloader-transition/m-p/2415878#M28628</guid>
      <dc:creator>NXP_007</dc:creator>
      <dc:date>2026-09-24T04:41:23Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775B – Application to RAppID Bootloader transition</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775B-Application-to-RAppID-Bootloader-transition/m-p/2416362#M28629</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/265056"&gt;@NXP_007&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As Peter said, you can't request&amp;nbsp; to run the bootloader from your application. The bootloader starts after each reset and it waits pre-defined time if it gets a response from RAppidBL application running on PC. If not, it starts the application.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The delay can be changed by user. See "2.7 RAppID Boot Loader Flash Algorithm (RBF)" in the user manual for details.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 25 Sep 2026 14:35:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775B-Application-to-RAppID-Bootloader-transition/m-p/2416362#M28629</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2026-09-25T14:35:10Z</dc:date>
    </item>
  </channel>
</rss>