<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FreeRtos on MPC-5668 in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/FreeRtos-on-MPC-5668/m-p/291237#M285</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Oct 2017 14:55:33 GMT</pubDate>
    <dc:creator>gorgiaslee</dc:creator>
    <dc:date>2017-10-27T14:55:33Z</dc:date>
    <item>
      <title>FreeRtos on MPC-5668</title>
      <link>https://community.nxp.com/t5/MPC5xxx/FreeRtos-on-MPC-5668/m-p/291235#M283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;i'm trying to port freeRTOS to mpc5668 microcontroller. I'm new in porting and i need every type of help how to write a port.c and portmacro.c , because its so important for me.&lt;/P&gt;&lt;P&gt;I'm using CodeWarrior and Lauterbach...I found port.c for mpc5xxx but for GCC, can anyone describe whats the differnce between this two compilers?&lt;/P&gt;&lt;P&gt; Thanks a lot&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Oct 2013 17:51:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/FreeRtos-on-MPC-5668/m-p/291235#M283</guid>
      <dc:creator>paulphilipp</dc:creator>
      <dc:date>2013-10-21T17:51:51Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRtos on MPC-5668</title>
      <link>https://community.nxp.com/t5/MPC5xxx/FreeRtos-on-MPC-5668/m-p/291236#M284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you're using CodeWarrior development tool to develop your application for MCP5668.&lt;/P&gt;&lt;P&gt;We've 2 versions supporting this device:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - CodeWarrior for MCU V10.5 based on Eclipse (most recent version),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - CodeWarrior for MPC55xx/56xx V2.10 based on classic IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for my understanding the development tools don't include GCC build tool chain.&lt;/P&gt;&lt;P&gt;Under the compiler manual there is a chapter for GCC extensions.&lt;/P&gt;&lt;P&gt;Please have a look to "\CW MCU v10.5\MCU\Help\PDF\MCU_Power-Architecture_Compiler.pdf"&lt;/P&gt;&lt;P&gt;Page 283: Chapter 15 - C Compiler&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We provide some header files for each processor.&lt;/P&gt;&lt;P&gt;this is used when you create a project with the wizard.&lt;/P&gt;&lt;P&gt;these files are in the folder:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; \CW MCU v10.5\MCU\lib\wizard_data\PA\DataBase\derivatives&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; \CW for MPC55xx and MPC56xx 2.10\bin\Plugins\Support\MPC55XXWizard\DataBase\derivatives&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We provide another tool which can be used&amp;nbsp; to generate the config file for the processor used.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RAPPID" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RAPPID"&gt;RAPPID Product Summary Page&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Details:&lt;/P&gt;&lt;P&gt;RAppID is a family of graphical development tools for the MPC5XXX family of Power Architecture® controllers that enables the user to quickly and easily configure the controller PLUS generate complete documentation. It can also be used as a learning tool to gain an understanding of the controller and it’s peripherals. RAppID not only generates C code for initializing the registers, but it also provides a system initialization function that brings the controller up in an orderly sequence. Use RAppID to save time and become an expert on the MPC5XXX Family.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Click on Download Tab and scroll down.&lt;/P&gt;&lt;P&gt;there is a version for:&lt;/P&gt;&lt;P&gt;&lt;A href="#"&gt;RAppID Pin Wizard for MPC5668E/G processors&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="https://community.nxp.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : RAppID Pin Wizard for MPC5668G/E processors. &lt;/P&gt;&lt;P&gt;&lt;SPAN class="sizeText"&gt;&lt;STRONG&gt;Size (K): &lt;/STRONG&gt;51223 &lt;STRONG&gt;Format: &lt;/STRONG&gt;zip &lt;STRONG&gt;Rev #: &lt;/STRONG&gt;0 &lt;STRONG&gt;Modified: &lt;/STRONG&gt;2/27/2009 &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;hope this will help you.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pascal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Nov 2013 13:02:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/FreeRtos-on-MPC-5668/m-p/291236#M284</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2013-11-08T13:02:32Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRtos on MPC-5668</title>
      <link>https://community.nxp.com/t5/MPC5xxx/FreeRtos-on-MPC-5668/m-p/291237#M285</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Oct 2017 14:55:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/FreeRtos-on-MPC-5668/m-p/291237#M285</guid>
      <dc:creator>gorgiaslee</dc:creator>
      <dc:date>2017-10-27T14:55:33Z</dc:date>
    </item>
  </channel>
</rss>