<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: AUTOSAR MCAL for MPC5744P</title>
    <link>https://community.nxp.com/t5/MPC5xxx/AUTOSAR-MCAL-for-MPC5744P/m-p/2396836#M28489</link>
    <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/13836"&gt;@petervlna&lt;/a&gt;&amp;nbsp;, is there any free compiler option to build the AUTOSAR MCAL applications for MPC5744P?&lt;/P&gt;</description>
    <pubDate>Mon, 20 Jul 2026 14:29:55 GMT</pubDate>
    <dc:creator>DanielFelix</dc:creator>
    <dc:date>2026-07-20T14:29:55Z</dc:date>
    <item>
      <title>AUTOSAR MCAL for MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/AUTOSAR-MCAL-for-MPC5744P/m-p/2097982#M27614</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I'm working with the MPC5744P and using the generated AUTOSAR MCAL packages.&lt;/P&gt;&lt;P&gt;I'm encountering a build error:&lt;BR /&gt;No such file or directory — referring to Os_memmap.h inside MemMap.h:&lt;/P&gt;&lt;P&gt;#ifndef AUTOSAR_OS_NOT_USED&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; #include "Os_memmap.h"&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;However, Os_memmap.h is not present in the generated files.&lt;/P&gt;&lt;P&gt;How can I get this missing file?&lt;/P&gt;&lt;P&gt;Also, how can I use EB tresos to configure and generate a new MCAL package (or regenerate the missing parts)?&lt;/P&gt;&lt;P&gt;Any help would be appreciated!&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Thu, 15 May 2025 08:56:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/AUTOSAR-MCAL-for-MPC5744P/m-p/2097982#M27614</guid>
      <dc:creator>MohamedElGreatly</dc:creator>
      <dc:date>2025-05-15T08:56:10Z</dc:date>
    </item>
    <item>
      <title>Re: AUTOSAR MCAL for MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/AUTOSAR-MCAL-for-MPC5744P/m-p/2098678#M27615</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;How can I get this missing file?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;It is not part of generated files of MCAL but from the Tresos OS configuration.&lt;/P&gt;
&lt;P&gt;In my opinion probably there was something wrong in OS configuration.&lt;/P&gt;
&lt;P&gt;Have a look also here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/No-such-file-or-directory-include-quot-Os-memmap-h-quot/td-p/1818413" target="_blank"&gt;https://community.nxp.com/t5/S32K/No-such-file-or-directory-include-quot-Os-memmap-h-quot/td-p/1818413&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;Also, how can I use EB tresos to configure and generate a new MCAL package (or regenerate the missing parts)?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Hmm, we offer S32 design studio for such. For trainings on Tresos please get in touch with Elektrobit.&lt;/P&gt;
&lt;P&gt;Actually it should be very simple. Once you install MCAL you will simply create project, add desired pluggins and generate the c/h files from tresos. Then you will put the project together in some project manager like S32DS, GHS, etc... to be able to compile it.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 16 May 2025 06:41:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/AUTOSAR-MCAL-for-MPC5744P/m-p/2098678#M27615</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2025-05-16T06:41:05Z</dc:date>
    </item>
    <item>
      <title>Re: AUTOSAR MCAL for MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/AUTOSAR-MCAL-for-MPC5744P/m-p/2099304#M27616</link>
      <description>Hi Peter,&lt;BR /&gt;Thank you for the clarification!&lt;BR /&gt;&lt;BR /&gt;Just a quick question: Is it possible to compile the generated code (from Tresos + MCAL) using GCC, or is it mandatory to use toolchains like S32DS or GHS?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;El-Greatly</description>
      <pubDate>Sun, 18 May 2025 11:09:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/AUTOSAR-MCAL-for-MPC5744P/m-p/2099304#M27616</guid>
      <dc:creator>MohamedElGreatly</dc:creator>
      <dc:date>2025-05-18T11:09:24Z</dc:date>
    </item>
    <item>
      <title>Re: AUTOSAR MCAL for MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/AUTOSAR-MCAL-for-MPC5744P/m-p/2099669#M27618</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You can use the generated code and compile it in GHS or DIAB.&lt;/P&gt;
&lt;P&gt;Always refer to supported compilators in release notes of the RTD and OS.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_0-1747642736488.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/338447i70A1789F8615A7AE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="petervlna_0-1747642736488.png" alt="petervlna_0-1747642736488.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 19 May 2025 08:19:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/AUTOSAR-MCAL-for-MPC5744P/m-p/2099669#M27618</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2025-05-19T08:19:20Z</dc:date>
    </item>
    <item>
      <title>Re: AUTOSAR MCAL for MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/AUTOSAR-MCAL-for-MPC5744P/m-p/2396836#M28489</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/13836"&gt;@petervlna&lt;/a&gt;&amp;nbsp;, is there any free compiler option to build the AUTOSAR MCAL applications for MPC5744P?&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jul 2026 14:29:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/AUTOSAR-MCAL-for-MPC5744P/m-p/2396836#M28489</guid>
      <dc:creator>DanielFelix</dc:creator>
      <dc:date>2026-07-20T14:29:55Z</dc:date>
    </item>
  </channel>
</rss>