<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックMPC5744P</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P/m-p/2379951#M28429</link>
    <description>&lt;P&gt;Here's the English translation of your question: &amp;gt; Why is it that when I modify certain register values of the MPC5744P through S32DS, only some of the embsys registers can be modified? When modifying certain RW register values, an error is reported: "Error: Error in ONCE status register during instruction execution."&lt;/P&gt;&lt;P&gt;为什么我通过S32DS去修改MOC5744P的某些寄存器的值也是只有部分的embsys registers寄存器能被修改。修改某些RW寄存器值时会报出Error : Error in ONCE status register during instruction execution？&lt;BR /&gt;将上述一段话翻译为英文&lt;/P&gt;</description>
    <pubDate>Thu, 11 Jun 2026 08:22:37 GMT</pubDate>
    <dc:creator>GENG</dc:creator>
    <dc:date>2026-06-11T08:22:37Z</dc:date>
    <item>
      <title>MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P/m-p/2379951#M28429</link>
      <description>&lt;P&gt;Here's the English translation of your question: &amp;gt; Why is it that when I modify certain register values of the MPC5744P through S32DS, only some of the embsys registers can be modified? When modifying certain RW register values, an error is reported: "Error: Error in ONCE status register during instruction execution."&lt;/P&gt;&lt;P&gt;为什么我通过S32DS去修改MOC5744P的某些寄存器的值也是只有部分的embsys registers寄存器能被修改。修改某些RW寄存器值时会报出Error : Error in ONCE status register during instruction execution？&lt;BR /&gt;将上述一段话翻译为英文&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jun 2026 08:22:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P/m-p/2379951#M28429</guid>
      <dc:creator>GENG</dc:creator>
      <dc:date>2026-06-11T08:22:37Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P/m-p/2380581#M28431</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Without knowing any details I will answer just generally:&lt;/P&gt;
&lt;P&gt;The error is NOT a register access error - It is a debug link failure triggered by your write&lt;BR /&gt;And that happens because those specific registers:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;cause reset&lt;/LI&gt;
&lt;LI&gt;are not accessible in current mode&lt;/LI&gt;
&lt;LI&gt;require unlock / clock / sequence&lt;/LI&gt;
&lt;LI&gt;or cannot be safely written via debugger&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jun 2026 06:53:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P/m-p/2380581#M28431</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2026-06-12T06:53:56Z</dc:date>
    </item>
  </channel>
</rss>